Technical FAQs

Ask a Question

Smart-UPS Cloud Connection Card – Supported UPS Models

Issue:
The Smart-UPS Cloud Connection Card can only be installed in compatible UPS devices.

Product Line:
Smart-UPS Cloud Connection Card (AP9649)

Environment:
All supported operating systems.

Resolution:

The below UPS models are compatible with the Smart-UPS Cloud Connection Card. NOTE: Your “XXX” UPS model prefix is printed on the label at the back of your UPS.
  • UPS devices with the SRT prefix, excluding SRT5KXLTJ.
  • UPS devices with the SMX prefix, excluding SMX3000RMJ2U.
  • UPS devices with the SMT prefix, excluding SMT1500C, SMT1500J, and SMT1500RM1U.

 
Was this helpful?
What can we do to improve the information ?