GYIK-ok böngészése



How many 0U accessory channels (RCC's) are included with NetShelter SX cabinets, and how manu PDUs can fit into them?
Resolution: All 1070 mm deep NetShelter SX cabinets have 2 0 U accessory channels.
acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
... install two 21 U side panels onto each NetShelter VS (900- mm ) or NetShelter VX ( 1070 - mm ) enclosure.
How many 0U accessory channels (RCC's) are included with NetShelter SX cabinets, and how manu PDUs can fit into them?
Resolution: All 1070 mm deep NetShelter SX cabinets have 2 0 U accessory channels.
acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
... install two 21 U side panels onto each NetShelter VS (900- mm ) or NetShelter VX ( 1070 - mm ) enclosure.
Can cable bridge partition/trough be installed across the top of a 300 mm or 600 mm InRow chilled water cooling unit?
... square holes in the roof of the 300 mm chilled water cooling units so there's nowhere to connect the tabs on the NetShelter cable partition ...
How is the rackmount U-space of a NetShelter cabinet or rack identified?
... any Rackmount device or enclosure - a U or unit of rack space is equivalent to 1.75 inches or 44.45 mm ...
How to remove NetShelter SX rear doors when installed in rows.
When NetShelter SX cabinets are bayed at 600 mm , if the cabinets are not leveled correctly it may be difficult to remove the right ...


Találatok 1 - 10 ennyiből: 74

Nem találja, amit keres?

Lépjen kapcsolatba ügyfélszolgálati csapatunkkal technikai támogatásért, panaszokkal kapcsolatos segítségért és más ügyekkel kapcsolatban.