GYIK-ok böngészése



Video: Troubleshooting no communication between UPS and PowerChute Business Edition
Troubleshooting Windows Serial Communications ... - using 2400 as the baud rate ...
How do I properly install/uninstall my SmartSlot accessory card into my UPS?
- The unit can be completely powered down, commonly referred to as a "braindead." ... Press and hold the off button for approximately five seconds to turn off the DC (battery) power. ... - The unit can be completely powered down, commonly referred to as a "braindead." ... All Symmetra 1 & 3 phase, Smart UPS VT, Galaxy 3500, and other 3 phase product lines
Where can I get support for APC and MGE Products?
... 25 0033- 3 0033-50 ... 6 0034- 1 0034-100 0034- 3 0035-100 ... E 0035- 3 0035- 3 M-E ... 2M- 1 E 0035nd- 3 M- 1 E 0039- ... ... E 0088- 3 M-E ... 2M- 1 E 0088nd- 3 M- 1 E 0100- ... 2M- 1 E 0226- ... 50 0334- 3 0377- 1 M 0377- ... M 0377- 3 M 0386- ... 25 0423- 3 0423-6 ...
NetBotz 750 | Configuring Network Settings
1 ) Connect a USB-A to Micro USB-B cable to the Console Port on the NetBotz appliance and a USB port on your computer. ... 3 ) Open a serial connection on your terminal emulator using the following connection parameters: ... Stop bits: 1 ... The terminal settings are correct as specified in step 3 . The correct cable is being used as specified in step 2.
Matrix-UPS run time theory
1 . Age of the batteries ... 3 . Number of battery packs ... A calibration might establish that at 40 volts DC the batteries are 2 minutes from reaching 39 volts (which is always the end of discharge). As the batteries age, the 2 minutes to shutdown point will climb the discharge curve to a much higher value and the estimated run time displayed will be decreased accordingly. ... There could be as much as 30% error (on a good calibration). To
Video: Data Center Expert | Managing Users
1 ) Within the ... 3 ) Fill in ... 1 ) Within the ... 3 ) Fill in ... 1 ) Within the ... 3 ) Edit 1 ) Within the ... 3 ) Click Delete 1 ) Within the ... 3 ) Select 1 ) Define a ... 3 ) Click the ... ... =Users, dc =dcim, dc =apc, dc =com EX: dc =dcim, dc =apc, dc =com 1 ) Within the ... 3 ) Select 1 ) Within the ... 3 ) Select 1 ) Within the ... 3 ) Select ... This is working as designed.
UPS fails Insulation Resistance Test (PAT Test)
Normally the Insulation Resistance value should be around 1 M ohm. ... If the test is done using a high voltage, 500v DC , the unit will also allow excess Voltage to flow to Earth (Ground) to protect the load but this will show as a drop in resistance for measurement applications. Most European Regulations e.g. IEE 16. edition, section 10. 3 . 3 , require all electronic components to be disconnected before carrying out such tests.
NetBotz 750 | Resetting a Lost Root Account Password
1 ) Connect a USB-A to Micro USB-B cable to the Console Port on the NetBotz appliance and a USB port on your computer. ... Stop Bits: 1 ... 3 ) Press Enter, repeatedly if necessary, to display the User Name prompt. ... The terminal settings are correct as specified in step 2. The correct cable is being used as specified in step 1 . ... 6) Log on as the Root user (root).
Video: How do I configure APC Network Management Card network settings?
... Environmental Monitoring Unit 1 (AP9312TH) ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... ... Network Management Card 3 (NMC3) ... ... Network Management Card 1 : ... Network Management Card 1 (AP9617, ... Network Management Card 1 (such as a AP78XX or ... ... Network Management Card 1 based devices are ... ... Card 2/ 3 ... Card 2 and 3 based devices (such as an AP8XXX Next ... AOS 5. 1 . 1 or higher, ... ... v5. 1 .5 or ... Configuration Option 1 - Device IP ...
LDAP/LDAPS Configuration with KVM1116P, KVM2116P, and KVM2132P Digital IP KVM Switches
1 . Install the ... 3 . Extend and ... 1 . On your ... 3 . Follow the ... 1 . Open a ... 3 . Open the ... 1 . Right click ... 3 . In the ... ... Active Directory Schema as the name for ... 1 . Create a ... 3 . Edit the ... 1 . From the ... 3 . Select New ... 1 . Open the ... 3 . In the ... 1 . Run ADSI ... (Installed as part of the ... ... navigate to the DC =domain , DC =com 3 . In the ... ... the same permissions as user. ... to be entered as the username for ...


Találatok 1 - 10 ennyiből: 83

Nem találja, amit keres?

Lépjen kapcsolatba ügyfélszolgálati csapatunkkal technikai támogatásért, panaszokkal kapcsolatos segítségért és más ügyekkel kapcsolatban.