Consulter la FAQ



What type of battery could I use with the Galaxy VS UPS?
Galaxy VS, 3 ... Supply,10 kVA ,15 kVA , 20 kVA , 20 kVA , 30 kVA ,40kva, ... use with the Galaxy VS UPS? ...
Video: How can the Galaxy VS reduce my energy bill?
Galaxy VS, 3 ... Supply,10 kVA ,15 kVA , 20 kVA , 20 kVA , 30 kVA ,40kva,50kva, ...
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
... – STS, Galaxy 3000 , 4000, 5000 and Galaxy PW ... – STS, Galaxy 3000 , 4000, 5000 and Galaxy PW The 66061 JBUS/Modbus card is configured for 9600, 8, N and 1 . Slave address is 1 and wiring is 2-wire with no parity and termination. This assumes only one 66061 card or UPS or STS is connected to the enclosure but if more than one change as required. ... The IP address needs to be configured at the site . ... One is down (off position) and all others are up.
Smart-UPS VT and Galaxy 3500 Power Off, Bypass and Power on Procedures
If applicable (Turn XR frame DC breaker on) Turn ON Q 1 (wait about 30 seconds.)
Batteries; Is it OK to replace the internal batteries or use refurbished modular battery modules?
Symmetra PX1 20 - 80 kva , Symmetra PX2 100 kva , Symmetra PX 250-500 kva , SUVT, ... , ais3000, Galaxy VM
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
Cause: Due to site maintenance, inclement weather, and other conditions, request come in for assistance with Powering Down the Galaxy 5000 UPS
Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS?
Issue: Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS
Network Management Card 660674/34003640se; ripple20 vulnerability status
Galaxy 5000, Epsilon STS, Upsilon STS, eps6000, eps7000, eps8000, Galaxy 4000, Galaxy 3000 , Galaxy PW, Comet ...
MGE NMC Card; Statement of Volatility (SOV) for the 660674/34003640se MGE NMC
Galaxy 5000, Epsilon STS, Upsilon STS, eps6000, eps7000, eps8000, Galaxy 4000, Galaxy 3000 , Galaxy PW, Comet ...


Résultats 1 - 10 de 50

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.