Consulter la FAQ



Data Center Expert | Obtaining an SNMP or Modbus DDF for discovery of third-party devices
Installing a Device Definition File within DCE 3) Proceed to .
File transfers may be unsuccessful using SCP on devices within StruxureWare Data Center Expert (DCE) with v6.X.X firmware earlier than v6.3.3
This may affect the transfer of the config,ini file or CSF file for device configuration. This does not affect firmware file transfers.
Video: Data Center Expert | How do I mass upgrade APC and NetBotz appliance firmware?
... Center Expert ( DCE ) - Basic ... ... ) Open the DCE desktop client and ... ... which selects all devices that require that ... or select individual device updates. ... When checking a device , ensure to ... ... that within the Device File Transfer Settings that ... credentials of the devices are listed with ... ... can not use DCE to push an ... version to a device . ... to download the catalog file . ... the reason that DCE does not have ... ... rule that allows DCE to reach the ... ... manually adding the device firmware catalog file into Data Center ...
How do I add a DDF to StruxureWare Data Center Expert?
In order to add devices to DCE , a device definition file or DDF must exist on the server.
Data Center Expert | Alarm "Device status may be inaccurate due to attempt to transfer DDF failed"
... Expert message " Device status may be ... ... Center Expert ( DCE ) - Basic ... APC Networked Devices ... Center Expert uses device definition files (DDFs) ... from a discovered device . ... discovery of APC devices and after a ... download a DDF file (ddf. ... ) from the device using either FTP ... ... message stating " Device status may be ... Device Definition File Transfer Process ... out to the device to pull down ... ... connect to the device using passive FTP ... defined within: DCE Desktop Client > Device menu > SNMP Device Communication Settings > Device File Transfer Settings.
Data Center Expert | Why is a device definition file (DDF) required from an APC device when some already exist on the system?
The alerts DDF is stored on the APC device and transferred to DCE when the device is discovered or if the device's firmware is updated ...
Data Center Expert | Application Version does not update in the UI after upgrading devices to AOS 6.4.6 and newer
In order to resolve the above symptoms, an update to a DCE Core DDF file is needed.
Data Center Expert | Lost communication to APC devices using snmpv3 communication when upgrading NMC AOS to v6.4.6
To re-establish snmpv3 communication, it is recommended to reboot your DCE server under the file menu within the desktop client.
Data Center Expert | Discovering a ModbusTCP device
If you device is not listed, ... need to obtain a Device Definition File (DDF) and add it to DCE before continuing.
Data Center Expert | Download the Essential Device Definition File (DDF) for NetBotz Rack Monitor 750
... Web UI password to download the essential Device Definition (DDF) file for the Rack Monitor 750 in StruxureWare Data Center Expert ( DCE ...


Résultats 1 - 10 de 90

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.