Browse FAQs



Information for Colors of UPS Galaxy 5000, Galaxy 5500
Environment: Galaxy 5000 40kva , 50kva,60kva, 80kva, 100kva and 130kva
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
... Down the MGE Galaxy 5000 UPS Galaxy 5000 , Galaxy 5500 ... Powering Down the Galaxy 5000 UPS ... power down the UPS are available on ... ... is for a single UPS without an external ... Step 1 : Touch any button on the display to wake it up. ... Step 4: Choose “Stop the UPS ” ... At this point, the load is no longer protected by the UPS . ... The UPS is now fully isolated from the load. ... Step 6: Turn the Q 1 Switch to Off ... There is still stored energy in the capacitors, and batteries inside the UPS . Never remove any covers or panels.
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from total power ... Galaxy 5000 , Galaxy 5500 ... reasons, the Galaxy 5000 may be in ... ... commissioning a new UPS . ... of a new UPS must be performed ... ... to restore the Galaxy 5000 UPS from total power ... This procedure is for a single UPS without an external bypass panel. ... Step 1 : Set the input Q 1 switch to On Step 2: Wait until the end of the UPS initialization with PFC start-up. ... Step 4: Choose “Start the UPS ” ... The Inverter Assumes the load, and the UPS is normal operation with the load protected.
​Information for Noise level of UPS Galaxy 5000 NAM
Environment: Galaxy 5000 40kva , 50kva,60kva, 80kva, 100kva and 130kva
Galaxy 5000; Modbus Q1 Input Breaker status does not change state
The Q 1 Modbus register is only monitored on EMEA Galaxy 5000 / 5500 UPSs.
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
This assumes only one 66061 card or UPS or STS is connected to the enclosure but if more than one change as required.
Galaxy 5000, Galaxy 5500; Dust Covers
... has been determined that dust and other foreign conductive particles have been getting inside the UPS during shipping or from site construction projects during installation ...
AP9635 Modbus registers are not compatible with NAM Galaxy 5000 Modbus registers
AP9635 Modbus registers are not compatible with NAM Galaxy 5000 Modbus registers. ... Galaxy 5000 NAM ... Galaxy 40kva , 50kva,60kva, 80kva, 100kva and 130kva ... AP9635 Modbus registers are not qualified for NAM Galaxy 5000 . ... Do not use AP9635 MODBUS resistor for NAM Galaxy 5000 UPS . Use below link to download the correct Modbus register used for NAM Galaxy 5000 .
Modbus Installation and Troubleshooting for AP9635/AP9635CH Network Management Card 2 (NMC2)
... Modbus TCP or Modbus RTU with AP9635/AP9635CH ( Galaxy VM, Galaxy 300/7000, Galaxy 5000 / 5500 , etc)


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.