我們的品牌

The Modbus protocol is a standard in the industry and is supported by almost all of the BMS vendors. APC integrates Modbus TCP over an Ethernet connection and Modbus RTU/ASCII over a serial connection for NetBotz® communication with a BMS (e.g. T.A.C Continuum™ and Vista™, Johnson Controls’ Metasys™, Siemens’ APOGEE™, ALC’s WebCTRL™, etc.). This paper explains the integration of the APC NetBotz® appliance v3.2 release with a Building Management System.

Tarih: 07 Aralık 2010 | Tip: Uygulama çözümleri
Diller: İngilizce | Versiyon: V1
Belge Referansı: SPD_JRUK-7UPPJ3_EN
İndir

Files

File Name
JRUK-7UPPJ3_R1_EN.pdf
JRUK-7UPPJ3_R1_EN_SRC.zip

İlgili ürünler

The Modbus protocol is a standard in the industry and is supported by almost all of the BMS vendors. APC integrates Modbus TCP over an Ethernet connec...

Tarih: 07 Aralık 2010
Tip: Uygulama çözümleri
Diller: İngilizce
Versiyon: V1

Files

File Name
JRUK-7UPPJ3_R1_EN.pdf
JRUK-7UPPJ3_R1_EN_SRC.zip
İndir actionLockOn Login or Create account to access

İlgili ürünler