Batteries; Is it OK to replace the internal batteries or use refurbished modular battery modules?
Symmetra PX1 20 - 80 kva, Symmetra PX2 100 kva, Symmetra PX 250-500 ... ... modules in my UPS ? ... Modules are factory assembled using new batteries ... Once assembled , the batteries ... ... one time use only . ... used by the UPS to identify the ... ... communicate with the UPS . ... alarms in the UPS , or a ... If we dispatch to troubleshoot faults that occur because of refurbished batteries, the visit would be billable regardless of contract or warranty status on the UPS or Battery frame. ... - Unauthorized modification of a component assembly voids the system UL/IEC/CE rating / listings.