How to navigate through an Network Air FM unit display
... MultiCool® ( chilled water ) and DX ... ... , then the cooling setpoint is used ... ... NetworkAIR FM DX 60 Hz Up to three Modules can be ... • Water ... avoid over- cooling while dehumidifying. ... valve which feeds three quarters of the ... ... the modes ( cooling , reheat, ... ... NetworkAIR FM DX 60 Hz Installation ... for fluid- cooled options ... of fluid- cooled option. ... (glycol or water ) flow to ... ... will switch the cool or dehumidify mode ... ... —for the water or glycol line ...