Browse FAQs



APC Schneider Cooling Unit Identification
APC Cooling Unit identification. All Cooling Units. All Product models , all serial ... Model ... W= Water Cooled ... F= Water Cooled ... D= Water Cooled ... G= Glycol Cooled ... B= Glycol Cooled ... P= Glycol Cooled Model ... coil C= Chilled Water Model C= Chilled Water ... In-Row Model ... Main C= Chilled Water Model ... W= Water Cooled ... G= Glycol Cooled BA=208 ... Model ... W= Water Cooled ... G= Glycol Cooled Model AFX 1 = 1 Bay ... Bay 06 ( 1 Bay) 08 ( 1 Bay)
DAC, Cancoil Installation Manual
All Models Section 1 . Warranty and ... Section 1 . ... designed to provide years of reliable performance ... stable, efficient year round operation for ... ... and dry and free of all debris ... ... are based on 1 degree per 100 ... ... a rate of 1 ” drop per ... ... page 8) plus the evaporator charge plus the suction line ... ... a rate of 1 ” drop per ... ... and should have 1 additional trap per ... ... information regarding the model in question. ... the system with 1 /4” ... 1 . Check the ... The ambient fan cycling controls will maintain a condensing temperature of about 115 degrees whenever the outdoor temperatures are greater than the values shown above.
Where can I get support for APC and MGE Products?
Air Cooled Chillers ... Data Center Facility Cooling - Andover Continuum or TAC Vista ... High-Density Cooling Enclosures ... InRow Chilled Water ... Planning Tools and Publications Portable Cooling ... PowerChute plus ... Room Cooling Accessories ... Row Cooling Accessories ... Service Plans ... Uniflair Chilled Water
Why are the battery charge LEDs flashing on a Smart-UPS?
... Smart-UPS models with model numbers ... Option 1 : ... submenu of PowerChute plus . ... to last for years , yet the ... ... Extended Run) model , then try ... Typical battery life is 3 - 6 years . ... Make sure a 30% load or greater is present! ... Remember that if the unit is an older model , then the runtime will not improve significantly. ... To ensure that an operating system receives a graceful shutdown when using PowerChute plus or a SmartSlot accessory, an alert is generated by the Smart-UPS indicating that the UPS has reached a low battery condition.
Schneider Electric's Technical Support Policy for Older Versions of PowerChute Software
PowerChute Plus ... When new versions of software are released, Schneider Electric will continue to provide full technical support to customers for the previous version for a minimum of 1 year after the new version is released. In practice, Schneider Electric typically goes far beyond this stated commitment, but this 1 - year policy is stated here so customers may take it into account for planning purposes. ... PowerChute Plus (PC+) was discontinued March 2007
What filter is being used for your InRow 300mm?
Data Center Cooling ... The filtration of conditioned air is extremely vital to maintaining the clean, particle- free environment required by electrical equipment. The system uses a <20% efficiency ASHRAE 52.1, 12.7 mm ( 1 /2 in) washable, deep loading, large dust-holding filter that meets HF- 1 standards for electronics (MERV 1 per ASHRAE 52.2). Model ... 1 acrc10x
Why choose glycol over water?
All cooling units that require heat exchangers ... All Product models , all serial numbers ... - Since glycol systems are closed and dirt- free , no sidestream or full flow filtration is required. ... - Did you know that just 1 /16" of scale reduces heat transfer by 40%!
Did APC purchase the AirFlow Company?
Data Center Cooling ... require a unit model and serial number ... American Power Conversion Expands Availability Solutions with Acquisition of Airflow Company Precision Cooling Acquisition Deepens Opportunities ... a leading precision cooling equipment manufacturer, ... million in cash plus the assumption of ... ... , global, one -stop shop ... ... , highly efficient cooling solutions," ... ... into the precision cooling business while leveraging ... ... million global precision cooling market. ... growth rate of greater than 30 percent ... ... are caused by cooling problems. Precision cooling solutions are specifically ... A precision cooling device goes beyond ... or "comfort cooling " equipment to ... ... its highly efficient cooling products, which ...
What is the RDU’s entering water temperature guidelines
All Product models , all serial numbers ... 1 . What range of Entering Water Temperature should be supplied for the system? ... Typically if you chilled water source is starting to exceed its target set point, the chiller will alarm and begin to inform you of the problem as well.
Water leak in DataCenter.
All DataCenter Cooling Units. All Product models , all serial ... One of the very ... If you find a sag in the tubing that makes the equivalent of a trap plus a real trap or any multiple combination of either of these in the same line it is a problem. Make sure the line drains consistently downward and only has one trap. ... This condition of suction can also cause the water to back-up in the line and cause an overflow of the pan. Trap it if it doesn't have one . ... section where it is explained in great detail.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.