Browse FAQs



3 Phase Products Service Level Agreements; Definition of coverage as relates to the service level agreements offered by SE
Definition of coverages as relates to the service level agreements offered by SE UPS & PDU On-Site Warranty Extension :
Which SmartSlot accessories are supported by the Galaxy 3500 (g3500) UPS?
... supported by the Galaxy 3500 (g3500) UPS ? ... Facility 3 Phase UPS MGE Galaxy 3500 models ... supported by the Galaxy 3500 UPS (g3500) ... ... Network Management Card 2 - ap9630/ ... ... Network Management Card 2 SKUs ap9630/ ... with the g3500 UPS . ... with the g3500 UPS . ... Network Management Card 2 to have dry ... functionality - ( 2 ) inputs, ... maximum of ( 2 ) ap9810 that ... AP9622 product page ... in the g3500 UPS . ... in the g3500 UPS . ... must use Configuration 2 , as mentioned ... ... front panel/ UPS door will not ...
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
... Down the MGE Galaxy 5000 UPS Galaxy 5000, Galaxy 5500 Due to site maintenance, inclement ... Powering Down the Galaxy 5000 UPS ... power down the UPS are available on ... This procedure is for a single UPS without an external bypass panel. ... Step 2 : Push the Menu Button ... Step 4: Choose “Stop the UPS ” ... At this point, the load is no longer protected by the UPS . ... The UPS is now fully isolated from the load. ... There is still stored energy in the capacitors, and batteries inside the UPS . Never remove any covers or panels.
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
... take the Single Galaxy 5000 UPS from normal operation ... Galaxy 5000, Galaxy 5500 Due to site maintenance, inclement ... Powering Down the Galaxy 5000 UPS ... power down the UPS are available on ... ... for a single UPS with an external ... Step 2 : Push the Menu Button ... Step 4: Choose “Stop the UPS ” ... At this point, the load is no longer protected by the UPS . ... The UPS is now fully isolated from the load. ... Step 11: Open the UPS door. ... There is still stored energy in the capacitors, and batteries inside the UPS . Never remove any covers or panels.
How to configure NetBotz version 2 external sensors?
It’s always a good idea to test the sensors and cabling before fully deploying the solution on-site .
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... and wiring is 2 -wire with ... ... 66061 card or UPS or STS is ... ... Modbus card has two female DB9 connectors ... ... configured at the site . The wiring of the devices is below and keep in mind that the 66061 JBUS/Modbus card has a female DB9 so a male DB9 cable is required on the UPS /STS. The male DB9 connector is not supplied with the UPS but a black terminal block is supplied with the EGX.
Video: How can the Galaxy VS reduce my energy bill?
Compared to a legacy design, the savings are equivalent to the UPS acquisition costs after only two years .
Why is my Web/SNMP (ap9606) or Network Management Card 1, 2 or 3 not recognizing my UPS or device?
Firmware Application Name Single or three phase Smart- UPS , Galaxy 3500, Matrix UPS
Serial communications between Smart-UPS VTs, Galaxy 3500, and Symmetra PX with IBM AS/400, i Series
this document If the UPS has two or more SmartSlots, you can refer to for the proper installation order of multiple accessories.
Modbus Installation and Troubleshooting for AP9635/AP9635CH Network Management Card 2 (NMC2)
... support Modbus TCP or Modbus RTU with AP9635/AP9635CH ( Galaxy VM, Galaxy 300/ 7000 , Galaxy 5000/5500, etc ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.