Safety Guidelines for Smart-UPS, BACK-UPS, and Surge products
Published date:
13 January 2021
Issue:
Safety Guidelines for Smart-UPS, BACK-UPS, and Surge products
Product Line:
Smart-UPS, Back-UPS, Surge
Environment:
All models, All Serial Numbers
Cause:
This document contains important instructions that should be followed during installation, operation, and maintenance of your Smart-UPS, Back-UPS, or Surge products
Resolution:
Read the operating instructions carefully and look at the equipment to become familiar with the device before trying to install, operate, service or maintain it.
The following special messages may appear throughout this document, the operation manual for your particular product, or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure.
Do not attempt to use the product if it shows signs of physical damage.
• Adhere to all national and local electrical codes.
• All wiring must be performed by a qualified electrician.
• Changes and modifications to this unit not expressly approved by Schneider Electric could void the warranty.
• Smart-UPS, BACK-UPS, and Surge products are intended for indoor use only.
• Do not operate units in direct sunlight, in contact with fluids, or where there is excessive dust or humidity.
• Be sure that any air vents on the product are not blocked. Allow adequate space for proper ventilation.
• The equipment may be heavy. Always practice safe lifting techniques adequate for the weight of the equipment.
Battery safety
• When replacing batteries, replace with the same number and type. Always replace all batteries at the same time, and only use official APC Replacement Battery Cartridges
• Batteries typically last for two to five years. Environmental factors impact battery life. Elevated ambient temperatures, poor quality utility power, and frequent short duration discharges will shorten battery life. Batteries should be replaced before end of life.
• Replace batteries immediately when the unit indicates battery replacement is necessary.
• Schneider Electric uses Maintenance-Free sealed Lead Acid batteries. Under normal use and handling, there is no contact with the internal components of the battery. Over charging, over heating or other misuse of batteries can result in a discharge of battery electrolyte. Released electrolyte is toxic and may be harmful to the skin and eyes.
Should you encounter swollen or leaking APC batteries, contact APC Support for guidance
• CAUTION: Before installing or replacing the batteries, remove jewelry such as wristwatches and rings.
• CAUTION: Do not dispose of batteries in a fire. The batteries may explode.
• CAUTION: Do not open or mutilate batteries. Released material is harmful to the skin and eyes and may be toxic.
De energizing safety
Smart-UPS and Back-UPS products contain internal batteries and may present a shock hazard even when disconnected from the branch circuit (mains).
Before installing or servicing the equipment check that the:
• Input circuit breaker is in the OFF position.
• Internal UPS batteries are disconnected.
Internal Batteries must be disconnected prior to shipment of the unit.
Should you have additional questions regarding the safe operation of your unit please contact APC Support
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.