Environment:
Windows 7 operating systems connected to NMC via the USB serial console cable
Solution:
Windows 7:
1. Connect USB
2. A device called “NMC3-CDC” is discovered in “Other Devices”
3. User must choose to update their device driver and manually select the path to the .inf file
4. User accepts unsigned driver security message
5. Windows associates the device with the usbser.sys driver and assigns a COM port
Windows 10: Windows 10 automatically makes the driver association and needs no manual intervention from the user.
1. Connect USB
2. A device called “NMC3-CDC” is discovered
3. Windows associates the device with the usbser.sys driver and assigns a COM port