Browse FAQs

Can a NetBotz Door Switch Sensor be installed onto NetShelter SX with RACS?

Published date: 15 October 2019

Issue:
There are no holes in the Rack Air Containment frame (front or rear) for the NetBotz Door Switch Sensor install onto. 

Product Line:
NetBotz NBES0301, NBES0302
HACS ACCS1006, ACCS1007

Environment:
All versions and serial ranges.

Cause:
The frame of the Rack Air Containment does not include the pre-drilled holes for NetBotz that the NetShelter SX does. 

Resolution:

The NetBotz Door Switch Sensors can be installed using the included 2-sided tape. Please see the attached document. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.