StruxureWare DCE may not show these formats correctly.
Resolution:
The attached apcsmartups_v71.zip file should be extracted and added to StruxureWare DCE. Go to the "Device" menu, "SNMP Device Communications Settings", and "Device Definition Files. If your current "APC SmartUPS version is 71 or above, you should not need to proceed.
If the version of the SmartUPS DDF is below 71, choose "Add/Update Definitions". Select "Local File" and hit the "Browse" button. Browse to the file apcsmartups.xml which was extracted from the zip file and hit open. Hit "Next" then select the DDF you just added and hit finish. The next time the device(s) are polled, you should see the new format.
Please note that this should affect all APC UPS models and not just the Smart-UPS line.