Video: Data Center Expert | Desktop Client Requirements, Download, & Installation
Published date:
05 August 2020
Issue:
Where can I find requirements and download the StruxureWare Data Center Expert desktop client software?
Product Line:
Struxureware Data Center Expert (DCE)
StruxureWare Central (SWC)
InfraStruXure Central (ISXC)
Environment:
Struxureware Data Center Expert (all versions)
StruxureWare Central (all versions)
InfraStruXure Central (all verisons)
Cause:
In order to discover devices and do most of the configuration required for DCE, you need to download and install the client application to your local system.
Information! This article only discusses downloading and installing the Desktop Client for the Data Center Expert software. For instructions on deploying the Data Center Expert Virtual Appliance on VMware, see knowledge base FA299551.
The StruxureWare Data Center Expert Desktop Client (console) is a stand-alone Java application that runs on systems that meet the following requirements:
A PC with a 1-GHz or better AMD/Intel processor running a 64-bit operating system: Microsoft® Windows® Server 2008, 2012, or 2016, Windows 7, Windows 8, or Windows 10; Red Hat® Enterprise Linux® version 6.0; CentOS 6
At least 1 GB of RAM
Screen resolution should be set to at least 1024 x 768.
Supported browsers: Microsoft Internet Explorer® 11; Edge; Mozilla® Firefox®; Google Chrome™ See Known issues for details about support for Internet Explorer and Edge.
NOTE: See the release notes for the most up-to-date information on system requirements.
Downloading the Desktop Client
1) Open the DCE Appliance web interface by entering the IP address or hostname in a web browser.
2) In the upper-right corner will be an option to Download Client. NOTE: In older versions, it may be on a different area of the web interface.
3) To continue you will need to Read and Agree to the license agreement.
4) Download the Binary.exe for the Desktop Client (application).
5) Run the downloaded execuatble file and follow the on-screen instructions.
6) Once the installation completes, you can launch to the Desktop Client using the Desktop Icon (if done during installation) or the Start Menu Option for StruxureWare Data Center Expert #.#.#.