Details Returned from NetBotz Devices via Advanced Device Crawlers
Published date:
26 May 2015
Issue:
Details Returned from NetBotz Devices via Advanced Device Crawlers
Product Line:
NetBotz
Environment:
NetBotz version 2 Advanced Device Crawlers.
Cause:
The following information can be queried via Advanced Device Crawlers for NetBotz appliances assuming the NetBotz DDF (Device Definition File) is installed on the server appliance and the client appliance is SNMP enabled. Please note that not all information listed below is available on all NetBotz models.
Resolution:
Model
Temperature
Humidity
Airflow
Audio Alarm
Door Switch
Camera Motion
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.