Consultar las preguntas frecuentes



In the NetShelter WX 6U Vertical cabinet, can the 2U UPS Mounting Bracket also be used on a 1U or 3U Smart-UPS?
Issue: It is unknown whether a 1U ot 3U Smart-UPS can use the 2U mounting rail.
Do the 800 mm wide NetShelter SV cabinets have 1U rackmount spaces in the vertical mounting rails?
Cause: It appears there may be a 1U punch out in the vertical mounting rails.
Smart-UPS C Series FAQ
... part number, they are available as dedicated Tower or Rack-Mount models in 1000 VA and 1500 VA capacities.
Differences between ap7xxx and ap7xxxb Series Rack PDU's
The new SKU's are as follows: Type Description SKU New SKU Metered ap7800 - Rack PDU, Metered, 1U ap7800
How is the rackmount U-space of a NetShelter cabinet or rack identified?
For Example, to mount a 1 U device, 3 ... the installed device 1 hole space up or down is incorrect and will lead ...
UPS Interface Expander 2 SmartSlot Card (AP9624) - Incorrect System Behavior for Some Master Server Control Functions
... greater) UPS 09.3 SMT 2U Rackmount UPS 09.3 SMT 1U Rackmount (follow "SMX 1500va or less ...
What are the typical uses for an EcoAisle System
● NAS Storage devices 1U Servers
ACSC1XX Spare Parts List
1 1U Airflow Management Blanking Panel Kit (Qty 2) Black
How do I update the firmware of my SRT, SMC, XU, XP, SMX, SMT, SMTL, SCL, SLC, SRC, CHS series Smart-UPS?
Devices that do *NOT* have upgradable firmware: These units are 120 V devices built prior to date code 1037. Date code is the first 4 numbers in your serial number.
How do I update the firmware of my SRT/SMC/XU/XP/SMX/SMT/SCL/SLC/SRC/CHS series Smart-UPS using the Firmware Upgrade Wizard?
Issue: These units are 120 V devices built prior to date code 1037. Date code is the first 4 numbers in your serial number.


Resultados 1 - 10 de 24

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.