Browse FAQs

MGE NMC Card; Statement of Volatility (SOV) for the 660674/34003640SE MGE NMC

Published date: 10 July 2020

Issue:
Statement of Volatility (SOV) for the 660674/34003640SE MGE NMC



Product line:
660674/34003640SE


Environment:
660674/34003640SE Network Management Card (NMC)


Cause:
Information about the 66074 NMC hardware volatility.



Resolution:

Below is the information about the volatility of the NMC.
Model Memory Type Memory Size Volatile or Non-Volatile Retain Information When power is turned off? Alterable in the field? Battery Backed up?
SST39VF1601-70-4C-EKE FLASH 1M*16 bit Non-Volatile Yes Yes No
EM636165TS-7G SDRAM 1M*16 bit Volatile No Yes No




 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.