Browse FAQs

Connecting to multiple version 3 NetBotz devices adds a com port for each device.

Published date: 21 July 2020

Issue:

Connecting a computer to multiple version 3 NetBotz devices adds a com port for each device.

Product Line:

NetBotz

Environment:

NetBotz version 3 appliances.

Cause:

When connecting to a version 3 NetBotz device via USB, drivers need to be installed so you can communicate to the device for initial communications or, in some cases, troubleshooting. This driver creates a com port so the USB connection can communicate as a serial port.

Each time you connect to a different NetBotz appliance, another instance of a serial port may be created so if you are configuring multiple units this way, you may create multiple com ports.

Resolution:

If you do not wish to manually remove all of these ports, the driver manufacturer (FTDI) has created a driver removal utility.

This file can be obtained here at http://www.ftdichip.com/Support/Utilities.htm

The sectioned marked ""CDM Uninstaller"" - Driver Removal Utility has the direct link to the downloadable file to remove the drivers and com port entries.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.