Issue:
General functions of a DG5.0 control platform Product line:
Airflow Environment:
Data Center Cooling Cause:
Resolution: MANUALLY ROTATE UNITS IN REDUNDANT UNIT GROUP using the following path in the unit addresses as the 1 unit:
Path: Config >> Enter >> Enter (curser at Custom Setup) >> Down Arrow >> Scroll to Page 21 >> Special
TOGGLE THROUGH UNITS IN A SHARED DISPLAY SETUP:
Path: Help and Network buttons at the same time
RESETTING/RECONFIGURING DG5.0 BOARD:
Path: Blank Button >> enter (curser will move to the model above Software) >> Temp. and Run Hours at the same time (curser will move below the Software Ver. # >> Down arrow >> enter
BACK DOOR PASSWORD:
Path: Blank button >> Network and Temp at the same time >> Down arrow >> this will take you to the section where you can view or alter the 2 level passwords
FACTORY MENU:
Path: Blank button >> Config. >> Enter >> Enter (Curser should be at the Custom Setup) >> Press Special and Config at the same time >> Hit the Down Arrow Key
CLEARING ALARM HISTORY:
Path: Alarm History >> Blank Button >> Help
ADDRESSING THE BOARD to the DISPLAY:
Path: Temp & Humid & Run Hours simultaneously
RESETTING THE CONTROLLER
- Press Blank => Press Enter => Press Temp. & Run hours at the same time … the cursor will move below Software Revision#=> Press UP/DOWN arrow => Press Enter >> Press Enter -Waiting to Reset msg … when the Config screen comes up choose the AC Unit >> Press Enter and scroll through the I/O Setup until the screen reads Cycle Power >> Please cycle power at the breaker of the unit
INSTALLING A NEW BOARD AND SETTING UP UNIT ADDRESS
- Set dipswitches on the board for the Display and the Clock Card (settings can be found in the manual)
- Power on the unit
- Hold down Temp, Run hours, and Humid at the same time
- Configure the I/O Board to the terminal address
- NOTE: if nothing shows up use the UP/DOWN to toggle
- Press enter to access P:01 – terminal 1 (ONE) should read according to dip switch settings which is found in the manual
- Set the unit according to Pr. (Private) or (Shared)
- Accept changes to Yes
- Reset the board
- Press Blank Red Button => Enter (you will see the cursor move to the Model)
- Press Temp and Run Hours at the same time and the cursor will move below Software Revision#
- Press the UP/DOWN arrow
- Press Enter <Waiting to Reset msg>
- When the Config screen comes up choose the AC Unit
- Press Enter and scroll through the I/O Setup until the screen reads Cycle Power.
- Please cycle power at the breaker of the unit
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.