Consulter la FAQ

Where can I locate product model and serial number for my APC 3 phase UPS?

Date de publication : 28 January 2018

Issue:
Where can I locate product model and serial number for my APC 3 phase UPS?
 

Product line:
Silcon DP300E, Symmetra MW, Symmetra PX, Smart-UPS VT, Galaxy 3500

 
Environment:
All models, all serial numbers
 
 
Information:
Each product has at least one way to obtain the product model and serial number, and in some cases 2 or even 3 different ways to obtain this information.
 
Silcon DP300E: found inside the UPS front door panel where the display is located will be a sticker with the serial and model information. Also may be found in the NMC (Network Management Card) web interface, the serial will be under the "about system".
 
Symmetra PX 20, 40, 80, and Symmetra PX2 48,100 and 160: physical serial number sticker found on the frame, behind the door where the display is located (by the card cage) as well as from the display under DIAGS then frame status and then the rev, sn, mfg date option you will see the UPS serial. Also may be found in the NMC (Network Management Card) web interface, the serial will be under the "about system".
 
Symmetra PX 250-500: physical serial number sticker found inside the IO frame where the display is located. Also found via the display touch screen; under the wrench symbol then system information you will find the serial there. Also may be found in the NMC (Network Management Card) web interface, the serial will be under the "about system".
 
Smart-UPS VT and Galaxy 3500: physical serial number sticker is found on the back of the product, the serial number can also be accessed via the display under the DIAGS option followed by system information. Via the NMC (Network Management Card) the serial will be under the "about system".
 
Symmetra MW:  Serial number can be found on the UPS display pannel door, just above the display touch screen and behind the small panel cover.
 
 
 

 

Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.