Consulter la FAQ

Can the condensate pump for the 600mm units provide more lift if the capacity is de-rated?

Date de publication : 17 July 2020

Issue:
Can the condensate pump for the 600mm units provide more lift if the capacity is de-rated?

Product line:
ACRP1XX, ACRP5XX, ACRD5XX, ACRD5XX.

Environment:  
All Serial Numbers.

Cause:  
Install, Repair.

Resolution:
The pump does have some degree of lift compensation as many other pumps do. As the head decreases, the pump volume is reduced. The maximum shutoff is 19ft of head. The data for flow versus lift follows:
 
 

Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.