Consulter la FAQ

Smart-UPS VT-G3500; what is Generator Charge (GEN CHRG) mode feature, how does it work?

Date de publication : 16 October 2018

Issue:
What is Generator Charge (GEN CHRG) mode feature, how does it work?

 
Product line:
Smart-UPS VT – Galaxy 3500

 
Environment:
All Product models, All serial numbers

 
Cause:
Generator Charge is for de-rating the power the UPS uses for charging the battery when supplied from a generator.

 
Resolution:
The GEN CHRG (Generator Charge) mode can be activated via the display: Main Menu>System>Gen Chrg. The generator must supply a signal to the UPS to reduce charge.
 
UPS TB J106, Pins 7 & 8 are for external charge control. When 7 & 8 are closed, the UPS charges batteries with a pre-defined percentage (0-100%) of the maximum charging power. To be used in generator applications, or if special codes requires control of charging. See page 36 attached file, install guide.

Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.