Consulter la FAQ



SNMP OIDs Required for Rack PDU 2G Products (AP86XX, AP88XX, AP89XX)
Issue: SNMP OIDs required for Rack PDU 2G products - which are correct?
For OSHPD Preapproval (OSP) of Smart-UPS and NetShelter VX or 2-Post Rack: is it required to install all of the Smart-UPS models shown in the test documents in order to meet OSHPD compliance?
Cause: The OSHPD Preapproval (OSP) document shows specific combinations of Smart-UPS installed into the cabinet/ rack for testing.
Can the ends of a NetShelter 2-post or 4-post rack be closed with panels?
Issue: The customer wants to close off the ends of their open rack for a clean look.
Rack PDU 2G (AP8XXX) Network Port Sharing Information
The Reset/Reboot web page has many additional reset/reboot options for Rack PDU groups.These
Can I change the input plug or reduce the cord length on my Rack Power Distribution Unit (Rack PDU) or Rack Automatic Transfer Switch (ATS)?
Rack Power Distribution Unit ... Rack Automatic Transfer Switch ... ... policy is provided for reference or documentation ... APC will continue to honor the product warranty on a Rack PDU or Rack ATS if a licensed electrician is used to change the input plug or provided the replacement plug has the equivalent ratings of the original APC supplied plug. ... For more information on UL markings, please see the attached document. ... APC Rack ATS and Rack PDU products have not been evaluated by safety agencies for hardwiring in the field and as such, customer modification of these products for hard wiring cannot be supported.
Register Map For NetBotz 200 and 250 does not include external sensor pod sensors.
Register Map For NetBotz 200 and ... ... the modbus output for the sensors connected ... SNMP output will work fine for these sensors and if using StruxureWare DCE, you can use it's modbus output capabilities (with the AP95MODBUS license ) to output the sensor pods for the 200 and 250. The 250, beginning with AOS v6.5.0/nb250 v6.5.0, now includes support for remote sensors, external sensor pods, rack access, and wireless sensors.
Video: Data Center Expert | How do I enable surveillance for NetBotz cameras?
... Data Center Expert for NetBotz cameras. ... NetBotz v3 Rack Appliance: 450 ... NetBotz Rack Monitor 750 (nbrk0750) ... This is for customers that require assistance in enabling surveillance for NetBotz cameras in DCE ... Each NetBotz camera requires one Surveillance license . You can verify the licensing that you have installed by going to: System Menu > Server Administration Settings > License Keys. There will be a specific license type of Surveillance Pack with a total column and a used column. ... Mark the check box for License Camera. ... Select the Post Mode that you would like to record the Surveillance clips for .
What sensors are supported by the NetBotz Wireless Sensor Pod 180 (nbpd0180) ?
... Door Switch Sensor for APC Racks - 12 ft nbes0303 NetBotz Door Switch Sensor for APC Racks - 62 in ... Door Switch Sensor for Third Party Racks - 62 in ... Door Switch Sensor for Rooms or Third Part Racks - 50 ft nbes0302 APC Temperature Sensor - 13 ft AP9335T APC Temperature ... Sensor - 13 ft (Only reports ...
Why is my AP561X KVM Switch Not Recognizing My Rack PDU for Power Management Integration?
Issue My ap5610, AP5615, or AP5616 KVM Switch is not recognizing the attached Rack PDU for Power Management.
Data Center Expert | Download the Essential Device Definition File (DDF) for NetBotz Rack Monitor 750
... the Web UI password to download the essential Device Definition (DDF) file for the Rack Monitor 750 in StruxureWare Data Center Expert ( ...


Résultats 1 - 10 de 97

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.