Consulter la FAQ



NetBotz | Hardware & Software Support Information and Limits
... Hardware Warranty & Software Support The NetBotz Rack Appliances 750 has a software /hardware support limitation of 5 years (2 years factory with 3 years of purchasable extensions ... ... Appliance, except for consumables, such ... Year 1 Year 2 Year 3 Year 4 Year 5 Year 6 Software Support & Hardware Support Factory Warranty Out of Support Out of Support The NetBotz Rack Appliances 250 has a software /hardware support limitation of 5 years (2 years factory with 3 years of purchasable extensions ... ... Appliance, except for consumables, such ...
KVM-SERIAL Configuration Information and Assistance
... -SERIAL Configuration Information and Assistance including module's DB ... pinout and general information Rack Accessories - KVM ... ... KVM-SERIAL applications ... is intended to help provide some of that information . ... the pinout configuration for the KVM- ... ... APC serial cable for communications), ... in the following manner . ( 1 ) part number 940-0024 or 940-1524 APC UPS Smart Signaling serial cable ( 1 ) part number 940-0103 APC null modem serial cable ... 2400 baud rate, 8 data bits, parity none, 1 stop bit, no flow control.
INFORMATION BULLETIN: Potential Issue with AP8XXX series Rack Power Distribution Units with rpdu2g v6.0.9 firmware
... feature may stop functioning properly. ... higher, available for download on apc ... Rack Power Distribution ... in rpdu2g firmware application v6. ... may degrade the Rack PDU functionality over ... Rack PDU will continue ... ... higher, available for download on apc ... ... Select Filter by Software /Firmware and ... ... embedded device ( Rack PDU, etc ... ... of the screen for AOS and APP : ... power cycling the Rack PDU if you ... button on the Rack PDU display. ... access to the Rack PDU ... a terminal emulation program (If a ... your terminal emulation program must support XMODEM protocol - ...
Rack PDU 2G (AP8XXX) Network Port Sharing Information
General information regarding the Network ... Capability of AP8XXX Rack PDU models Rack Power Distribution AP8XXX Rack PDU series only ... ability to share one IP address via one network connection) General information ... to the detailed information sections below. ... up to four Rack PDUs using only one ... by connecting the Rack PDUs via the ... ports on the Rack PDU front panel ... All Rack PDUs in the ... using the same Rack PDU firmware revision ... in order to support the Network Port ... ... a number, 1 to 4, ... uniquely identify the Rack PDUs in a ...
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... such as a Rack PDU, AV ... ... with the wrong application and you need ... load the correct application . ... Environmental Monitoring Unit 1 (AP9312TH) ... ... Network Management Card 1 - AP9617, ... ... Network Management Card 1 include (but ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... For users upgrading ( ... ... pertain to your application . For example, if ... Symmetra 1 phase (Symmetra ... ... /tools/ software -firmware ... Filter by > Software / Firmware
Video: Data Center Expert | Desktop Client Requirements, Download, & Installation
... download the StruxureWare Data Center Expert desktop client software ? Struxureware Data Center Expert (DCE ... Struxureware Data Center Expert (all ... ... the configuration required for DCE, you ... install the client application to your local ... ... Minimum System Requirements for the DCE Desktop ... Information ! ... the Desktop Client for the Data Center Expert software . For instructions on deploying the Data Center Expert Virtual Appliance ... The StruxureWare Data Center Expert Desktop Client ... ) is a stand -alone Java application that runs on ... ... PC with a 1 -GHz or ... At least 1 GB of RAM
Creating an Aggregate Device within the KVM Access Software
... KVM Access Management Software and why it ... KVM Access Software (ships with ... ... their KVM Access Software All software versions ... ports into a single Aggregate Device, ... counts as a single node, and only requires a single license. ... case of utilizing Rack PDU Power Integration ... making it easier for the end user ... ... together to make for ease of management through the Access Software . When a ... ... ports/outlets for a total of ... ... the KVM Access Software . 1 .) Within ... ... you are adding one of the specifically ...
Did APC purchase the AirFlow Company?
Data Center Cooling ... purchased Airflow in 2000 and formed a ... Our Tech line will also ... American Power Conversion Expands Availability Solutions with Acquisition of Airflow Company ... October 23, 2000 - American Power ... equipment manufacturer, for $22. ... ... , global, one -stop shop of availability solutions for the fast- ... ... does the demand for compact, highly ... ... efficiencies, management technology and brand recognition ... ... are specifically designed for applications that are sensitive ... IT and telecommunications applications . ... " equipment to help enhance availability of ... ... a variety of applications including datacenters, ... ... throughout the industry for its highly efficient ... minimize the need for additional equipment to ...
Does my APC network enabled device support RADIUS or LDAP?
... network enabled device support RADIUS or LDAP ... ... Switched/Metered Rack PDU (AP78XX ... , and Netbotz Rack Access PX ( ... ... RFC (Request For Comments) standards for RADIUS authentication. ... devices do not support LDAP, or ... of authentication except for local device authentication ... ... party tools and software that will allow ... ... (LDAP as one possible example) ... ... refer to your software server vendor for information on integrating RADIUS ... Microsoft provides information regarding integration into ... Information on other LDAP ... ... and does not support nor recommend the applications listed or any ... ... "AS IS" basis as this information ...
Video: Why is my AP8XXX Rack PDU reporting communications lost with Phase Meter?
My AP8XXX Rack PDU is periodically ... Rack PDU: Communications ... Rack PDU: Component ... Rack PDU: Communications ... Rack PDU: Component ... ... the model of Rack PDU, you ... see multiple events for communication established/lost for Phase Meter 1 , Phase Meter ... ... and 0V for incoming voltage while ... AP8XXX Rack Power Distribution AP88XX Metered Rack PDU ... Metered By Outlet Rack PDU AP89XX Switched Rack PDU ... Metering By Outlet Rack PDU ... communication with the Rack PDU monitoring hardware ... ... timeout within the Rack PDU's internal communications ... Verify the Rack PDU firmware is ... visiting and looking for the latest SFRPDU2G


Résultats 1 - 10 de 85

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.