MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
Wiring information for egx100 to any 66061- ... ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW Wiring information for egx100 to any 66061- ... ... card is configured for 9600, 8 , N and 1 . Slave address is 1 and wiring is ... ... This assumes only one 66061 card or UPS or STS is connected to the enclosure but ... ... card is RS232 for configuration. ... must be wired to . ... IP address needs to be configured at ... One is down ( ...