What is Peak Surge Current rating?
Resolution : ... The current is then boosted (say x+100a) remeasured, tested, remeasured, ... When the 100ma measurement falls outside the +/- 10% allowable window, the last kA measurement was valid. ... You will see a lower kA rating with the 2 impulse because the part has already been hammered once , it is warmed up , the material within the part has not completely 'reset' itself , and