Consulter la FAQ



While connecting the battery terminals of the APC AV device, the terminals don’t always appear to line-up and in some cases the black plastic tags break-off.
The battery cartridge connections of the RBC63, apcrbc107 / 108 and SBATT are very ridged and difficult to manipulate.
How do I recycle APC batteries in the US and Canada?
Issue: How do I recycle APC batteries in the US and Canada?
What is the expected life of my APC UPS battery?
Most APC batteries should last three to five years. There are many factors which affect Battery life including environment and number of discharges.
Why should I use only genuine APC Replacement Battery Cartridge (RBC) in my APC UPS?
Using of a non- APC battery may result in lower runtime, damage the UPS, create hazardous conditions, or void safety certifications ...
Why aren't alarms clearing in the BMS (Battery Management System) AP9921X-AP9922 after replacing batteries?
After changing a battery in a string which is monitored by the APC Battery Management System, it is imperative to clear the old baseline ...
Complying with U.S. Department of Transportation (DOT) Shipping Regulations for Sealed Lead-Acid Batteries
All the batteries APC ships meet the requirements of UN Number 2800 ("" Batteries , wet, non-spillable"") ...
Video: What to do if the system is missing native shutdown battery options / How to restore HID UPS device driver.
... HID driver (Human Interface Device) being updated from HID UPS to APC UPS or APC Battery BackUP.
Battery Discharge During Storage
APC Batteries should be charged to 100% within 6 months of purchase by the end user.
Where do I find information on electrolyte contained within the SYBTU1-PLP and SYBTU2-PLP type APC, and/or the SE modular batteries such as GVSBTU, GVSBTHU and GVSBTHULL
... within the SYBTU1-PLP and SYBTU2-PLP type APC modular batteries , and/or the SE modular batteries such as GVSBTU, ...


Résultats 1 - 10 de 97

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.