Browse FAQs



Is it possible to convert a NetShelter SX Networking cabinet into a standard NetShelter SX cabinet?
Remove all four existing vertical mounting rails, including the finger-style cable managers in the front and the mounting flange on the left ...
Can the vertical cable trough from the rear of the front left hand rail of a NetShelter Networking cabinet be moved to the left hand side, or is there a version that installs onto the right hand rail?
... asking if the vertical cable trough can be ... NetShelter SX Networking cabinets. ... rail of a NetShelter Networking cabinet, using the same vertical cable duct as the ... The vertical cable trough that's installed ... rail in a NetShelter Networking cabinet cannot be ... The NetShelter Networking cabinets are designed ... Each NetShelter Networking cabinet ships with a set of Airflow Management Panels that are used to block any open areas above or below where a side airflow duct kit is installed. ... For a 48U cabinet please use 0M-10804.
Can the vertical cable management fingers for 600mm wide NetShelter cabinets be installed into 750mm wide NetShelter cabinets?
... into a wide NetShelter SX or SV. NetShelter SX and SV ... shows that these cable managers are not compatible with the wide SX or SV cabinets ... ... the 600mm wide NetShelter SX cabinets, so ... In the SX cabinets a better choice may be the ar7580a (42U), AR7585 (45U) or AR7588 ( 48U ) because they offer far more capacity. In the SV cabinets AR7721 and AR7723 are currently the only finger-style vertical cable managers available.
Can the horizontal cable troughs ar8008blk and ar8016ablk be used in conjunction with vertical cable managers ar7580a, AR7585 and AR7588?
... on the horizontal cable troughs will mount ... the rails when vertical cable managers ar7580a, AR7585 ... NetShelter SX Wide cabinets, vertical cable management and horizontal ... ... All 750mm wide NetShelter SX cabinets: ar7580a ... ... to use both vertical finger-style vertical cable managers and horizontal cable troughs on the ... a 750mm wide NetShelter SX cabinet. ... , when using vertical cable managers such as ar7580a ... still install the cable troughs which run ... ... holes in the cable managers and prevent hot ... ... finger-style cable managers are a 2 ... fully populate one vertical mounting rail in ...
Can vertical cable managers or 0U accessory rails be installed in the front and rear of a NetShelter SX cabinet?
Issue: Customers want to know if there is flexibility in installing vertical cable managers , or where to mount the 0U accessory rails.
What effect, if any, do the magnetic panels of the Vertical Exhaust Duct Kits have on high speed network cables?
Issue: The NetShelter SX Vertical Exhaust Duct Kits include magnetic panels.
Which NetShelter SX cabinet has a greater cable capacity, 750mm wide or 800mm wide?
Resolution: The 750mm wide and 800mm wide cabinets use the same vertical cable managers so they have the same cable management capacity.
Can ar7580a be installed into the 45U NetShelter SX?
We need to determine if the 42U finger-style vertical cable managers will fit into a 45U NetShelter SX cabinet. ... NetShelter SX , NetShelter Vertical Cable Management ... Availability issues with AR7585 may create the need to use 42U cable managers . ... ar7580a will install into the 45U NetShelter SX cabinet but there will be no cable management fingers U-spaces 1 thru 4 . Mounting it in this manner will allow the thru-holes of the mounting rails and cable managers to align.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.