Why doesn't StruxureWare or ISX Manager's mass configuration feature update or show password credentials on APC Network Management Card devices?
... ISX Manager or StruxureWare may not work ... ... devices with an integrated card), ... In NMC2 (ap9630, AP9631, AP9635, or any devices with an integrated card) v5.X.X, the passwords are also not stored in this configuration file. ... The config.ini file could be manually configured outside of ISX Manager to include the password using the information from the [SystemUserManager] section above. ... If you have ISX Central or StruxureWare Data Center Expert, this should not be an issue.