Browse FAQs



Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from ... Galaxy 5000, Galaxy 5500 ... reasons, the Galaxy 5000 may be ... ... to restore the Galaxy 5000 UPS from ... ... is for a single UPS without an external bypass panel. Step 1 : Set the input Q 1 switch to On ... initialization with PFC start-up . Step 4: Choose “ Start the UPS” Step 5: Turn the Q4S Switch to On Step 6: Turn the output switch Q5N to On Step 7: Turn the maintenance bypass switch Q3BP to Off ... Step 9: Press the Green “Inverter Start Button”
Where can I get support for APC and MGE Products?
Assessment Services ... Battery Replacement Services ... Ethernet Switches ... Installation Services ... KVM Switches ... Maintenance Bypass Panels ... MGE EPS 7000 ... MGE Galaxy MGE Galaxy 300 MGE Galaxy 3000 MGE Galaxy 3500 MGE Galaxy 4000 MGE Galaxy 5000 MGE Galaxy 5500 MGE Galaxy 6000 MGE Galaxy 7000 MGE Galaxy 9000 MGE Galaxy PW ... MGE Service Bypass ... MGE Static Transfer Switches ... Network Integration Services ... On Site Service ... Operations Change ... Project Management Services ... Rack-mount Transfer Switches ... Remote Monitoring Services ... Service Bypass Panel Service Plans ... Start-Up Service
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
Step 5: Press the Inverter OFF (gray) button for 3 seconds to transfer the load to the Static Bypass Switch .
Smart-UPS VT-Galaxy 3500; Bypass Not Available Input Freq/Volt Out Of Range, Output: Inverter sync. to bypass alarms
... UPS VT- Galaxy 3500; Bypass Not Available Input ... ... UPS VT- Galaxy 3500-ais3000 ... acceptable range for bypass operation. ... and indicates that static Bypass operation may not ... If the Bypass frequency is out ... ... the UPS to bypass . ... you to enter Static Bypass operation, it was because the bypass frequency was already ... Bypass Sync Error ... - 0, 1 % ... - 0, 1 % Bypass input voltage threshold ... ... Inverter sync to bypass error: ... synchronized to the bypass . ... PLL and the bypass voltage is above ... to go to bypass .
Smart-UPS VT and Galaxy 3500 Power Off, Bypass and Power on Procedures
... UPS VT and Galaxy 3500 Power Off, Bypass and Power on ... ... Ups VT, Galaxy 3500 ... Ups VT and Galaxy 3500 Power off/ bypass /power on ... UPS BYPASS PROCEDURE WITHOUT BYPASS CABINET ... “UPS into Bypass ”, Confirm ... Flip Mechanical Bypass Switch on front ... ... now in mechanical bypass UPS Bypass Procedure IF YOU HAVE BYPASS CABINET ... “UPS into Bypass ”, Confirm ... ... are in maintenance bypass with UPS in static bypass . Turn Q 1 to OFF position ... UP SEQUENCE WITHOUT BYPASS CABINET If bypass light is currently ...
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
... Down the MGE Galaxy 5000 UPS Galaxy 5000, Galaxy 5500 ... Powering Down the Galaxy 5000 UPS This procedure is for a single UPS without an external bypass panel. ... Step 1 : Touch any button on the display to wake it up. ... Step 5: Press the Inverter OFF (gray) button for 3 seconds to transfer the load to the Static Bypass Switch . ... Step 6: Turn the maintenance bypass switch Q3BP to ON. Step 4: Turn the output switch Q5N to OFF. ... Step 6: Turn the Q 1 Switch to Off Step 7: Turn the Q4S Switch to Off
What is the warranty on an ACSC1XX?
parts only. However, if start-up is purchased, the warranty changes to 1 yr.
Default password of 1234 does not work on the Display of new Galax VX or Galaxy VM.
... Galax VX or Galaxy VM. Galaxy VX, Galaxy VM ... ender user to change the password when first logging into a ... The display of the Galaxy VX and VM is part of the NMC and has been disabled. ... Serial port setting: for 9600 bps, 8 data bits, no parity, 1 stop bit, and no flow control. ... Enter password customer would like or enter apc so it can be changed later. ... You will be asked to change the password which can be changed or reenter apc.
How do I connect a EPO (Emergency Power Off) circuit to Galaxy VX?
How do I connect a EPO (Emergency Power Off) circuit to Galaxy VX? ... Galaxy VX ... How do I connect a EPO (Emergency Power Off) circuit to Galaxy VX? ... http://www.apcmedia.com/salestools/MBPN-A35JB8/MBPN-A35JB8_R 1 _EN.pdf?sdirect=true ... software) to have the UPS go to static bypass on EPO (default setting is no).
Which SmartSlot accessories are supported by the Galaxy 3500 (g3500) UPS?
... supported by the Galaxy 3500 (g3500 ... MGE Galaxy 3500 models ... supported by the Galaxy 3500 UPS ( ... ... inputs, ( 1 ) output per ... ... AP9613 utilizing dip switch configurations only) ... ... In order to avoid this issue, ... 1 .) Purchase ... 2.) Utilize an APC ap9600 single slot SmartSlot expansion chassis and extend the cable to the ap9600 with a 940-1500 serial cable. ... Also, if do not want to use the included accessory board, you can make your own cable, using the pinout in the ap9610 user's guide and avoid buying a right angle 25 pin extension cable.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.