Technical FAQs

Ask a Question

Filter results

    acpa4000 Spare Parts List
    0w3401 Pwr Cord, 3M iec309-16A TO C19 V- LOCK (OPTIONAL Power Cord Black
    How deep must the ar7580a Cable Manager be installed so the AR7581A Hinged Cover can open 90 degrees?
    ... .5" deep in order for the AR7581A hinged cover to open a full 90 degrees .
    Safety shuddered outlets will not accept a plug
    Plugs that have cord at a 90 degree angle to their prongs (right-angled plugs) can be more difficult to insert than ...
    NetworkAIR FM 3-Way Valve Flow Pattern
    ... a 24 VAC/VDC power supply That feeds the motor and drives the valve 90 degrees until the limit switch is tripped.
    Is there a door handle available that has two locks?
    Cause: A customer may want two locks as an extra level of security.
    Uniflair safety information
    Before performing any work on this unit, ensure electrical power is locked out and tagged out.
    Does the ACSC automatically restart after a high head pressure alarm?
    ... within 30 minutes, the ACSC will go into Persistent High Discharge alarm and will lock out the compressor.
    NetBotz 250 | Managing Users
    Note: A Super User account cannot be locked out , but can be manually disabled if necessary.
    How large can an power surge (electrical transient) be?
    Electrical industry standards indicate, electrical power surges inside a building can reach levels up to 6 ... deliver up to 90 joules of energy.
    How to I monitor NetBotz alarms using Modbus?
    So with this information, I opened a door with a locked handle and the information I ... alarm and it is an error level .
    Results 1 - 10 of 50