Technical FAQs

Ask a Question

Filter results

    Is COO, HTTS or ECCN information available for NetShelter CX cabinets and accessories?
    ar4038x431 NetShelter CX 38U 750 mm Wide x 1130 mm Deep Enclosure Dark Grey Finish
    Which NetShelter SX cabinet has a greater cable capacity, 750mm wide or 800mm wide?
    Issue: A customer asks if the 800mm wide NetShelter cabinet has a larger cable management capacity.
    Is there documentation available that shows the rackmount depths for Dell products?
    ... has other notes regarding compatibility of these rail kits, specific to the NetShelter SX 600mm W x 1070mm D cabinets.
    Is there a depth extender for the rear or front of NetShelter SX cabinets? Is there a way to bay the rear of cabinets that are different depths?
    The roof of the depth extender is not load bearing. Do not run cables, troughs or ladders atop the depth extenders.
    Can the NetShelter SX cabinet be purchased with no sides, doors, roof or other configuration?
    NetShelter SX cabinets are available in custom configurations. The most common configurations already have part numbers called X -options.
    Can the AR8125 NetShelter AV Sliding Shelf be installed into an SX cabinet?
    ... install the AR8125 NetShelter AV Sliding Shelf into an SX cabinet. NetShelter SX ... holes of the NetShelter AV cabinets. ... installed into an SX cabinet with square ... ... Will the AR8125 NetShelter AV Sliding Shelf Fit Into SX Cabinets? ... compatible to the SX series of cabinets ... In the NetShelter Compatibility Chart the ... ... mounted into an SX cabinet, or ... ... AR8125 into an SX cabinet? ... use with the NetShelter AV cabinets which ... ... rails to the NetShelter AV’s #10 ... ... AR8125 to a NetShelter SX with square holed ... ... ship with the NetShelter SX cabinets it won’t ...
    Is there a blank NetShelter door badge available? If so, what size is available and how many are in the package? Can APC provide custom door badges?
    NetShelter SX ... We offer sku ar7001x384, which is a pack of 40 blank door badges, The door badge is oval, and the dimensions are 71.5 mm wide x 39.4 mm high.
    Is it possible to convert a NetShelter SX Networking cabinet into a standard NetShelter SX cabinet?
    You may leave it. If you want to replace it you'll find the NetShelter SX roofs in the NetShelter Compatibility Chart.
    Results 1 - 10 of 50