NetBotz | Why does my wireless sensor pod nbpd0180 show an incorrect serial number when set up as a coordinator?
Wireless sensor pod 180 set as coordinator shows incorrect serial ... NetBotz NetBotz wireless sensor pod 180 ... ... you disconnect a wireless sensor pod that ... been connected via USB to the NetBotz appliance and configured as a coordinator and replace it ... pod, the NetBotz appliance will not ... ... make sure the NetBotz appliance properly shows ... ... loss from the router or end devices ... ... . Once the coordinator is disconnected go ... ... . Plug the coordinator back into the ... ... it as a coordinator again ( Wireless Sensor Pod 180 ... 4. Wait for the end devices and routers to report back into the coordinator and ...