Technical FAQs

Ask a Question

Filter results

    NetBotz 750 | What parts come with the NetBotz 750?
    Quantity Temperature / Humidity Sensor (AP9335TH) 1 Wireless temperature sensor (nbws100t) 1 Basement mount hardware kit (0M-814726) 1
    What sensors are supported by the NetBotz Wireless Sensor Pod 180 (nbpd0180) ?
    NetBotz Door Switch Sensor for APC Racks ... 12 ft nbes0303 NetBotz Door Switch Sensor for APC Racks ... 62 in nbes0313 NetBotz Door Switch Sensor for Third Party ... 62 in nbes0312 NetBotz Door Switch Sensor for Rooms or ... ft nbes0302 APC Temperature Sensor - 13 ft AP9335T APC Temperature & Humidity Sensor - 13 ft (Only reports temperature when connected to the nbpd0180 AP9335TH NetBotz Temperature
    What sensors come with the netbotznbrk0250 ?
    Not all sensors are shown in documentation ... Netbotz ... Temperature sensors are not shown in the inventory documentation. ... The nbrk0250 comes with one wired universal Temperature and humidity sensor , AP9335TH, and one Wireless Temperature Sensor (nbws100t) Neither are shown in the inventory within the Installation and quick configuration documentation. ... http://www.apc.com/shop/us/en/products/ NetBotz -Rack-Monitor-250/P-nbrk0250
    NetBotz 750 | Physical Description
    ... Description of the NetBotz 750 NetBotz version 5 NetBotz v5. ... ... connected devices ( sensor pods, rack ... pods, and temperature / humidity sensors with digital displays ... ... for connecting a NetBotz Leak Rope Sensor (nbes0308) ... ... the door switch sensors (nbes0302 or ... ) and handle sensors (NBHN125 or ... 6 Universal Sensor ports Used to ... by Schneider Electric sensors , third- ... dry-contact sensors , and standard ... -5 V sensors .
    Storage Temperature Range for All NetBotz Version Appliances
    Note:* Humidity sensor re-hydrating times may be necessary after prolonged exposure to extreme high temperatures and low humidity .
    NetBotz v3 | Unplugged Sensor Alarm
    NOTE: A temperature and humidity sensor will also have a dew point sensor .
    NetBotz 200 shows phantom sensors when multiple dry contact cables are connected.
    This does not effect temperature / humidity sensors and you can have other sensors connected at the same time as the 2 dry contact cables ...
    What is the range for Netbotz wireless sensor range?
    Supported devices on the NetBotz wireless network The Wireless Temperature Sensor is always configured as an End Device in your wireless sensor network.
    NetBotz 450/550/570 | Physical Description
    13 A-Link port Used for cascading NetBotz sensor pods and temperature and humidity sensors with digital displays.
    NetBotz 355 | Physical Description
    1 Vented internal sensors Vented opening for airflow, temperature , and humidity sensors . 2 Network link LED Shows the status of the network connection.
    Results 1 - 10 of 50