Can I use a NetBotz Camera Pod 160 nbpd0160 / nbpd0160a as a standalone appliance?
... of using a NetBotz camera pod 160 ... NetBotz NetBotz The NetBotz Camera Pod 160 ... connection to a Rack Monitor 450, ... 570, or Room Monitor 455. ... is for the NetBotz door sensor . The camera can not be discovered by StruxureWare without a connection to a main NetBotz appliance. ... Purchase a Rack Monitor 450, 550, or 570, or Room Monitor 455 for functionality. If the camera is the nbpd0169a, please be sure you upgrade to version 4.6.2 or higher of the NetBotz Firmware (also known as BotzWare).