Technical FAQs

Ask a Question

Filter results

    What are your condenser clearances and placement requirements?
    All Cooling Condensers Data Center Cooling ... supply of ambient air to the condenser ... removal of heated air from the condenser ... Units must not be ... steam, hot air or fume exhausts ... ... is that the unit should be mounted away from noise ... Units should be mounted over corridors, ... ... Along with proper mounting and isolation the ... ... need to be mounted on a safe ... ... present, proper mounts will be required ... ... and damage the unit or piping. Height Requirement ... feet above the unit providing all other ... Walls or Obstructions The unit should be located so that air may circulate freely ...
    DAC, Cancoil Installation Manual
    DAC Cancoil Installation manual Product line ... Install Installation and Operating Instructions ... equipment, proper installation and set- ... ... provided in the unit . DO ... SECTION OF THE UNIT . Unit Placement and Mounting - unit should be securely ... ... clearance around the unit for proper servicing ... Installation Date __ ... ... and dry and free of all debris ... Discharge Line - The discharge line should be ... Discharge Line – cont’d Discharge Risers – Discharge risers should be ... ... properly sized and installed to insure oil ... ... insulated to minimize external heat gain and ... ... risers should be installed with a trap ...
    APC Schneider Cooling Unit Identification
    APC Cooling Unit identification. All Cooling Units . APC Unit Identification FM Air /Water/ ... Air Pattern ... W= Water Cooled ... F= Water Cooled ... D= Water Cooled ... G= Glycol Cooled ... B= Glycol Cooled ... P= Glycol Cooled U= Upflow R= Upflow Air Pattern ... coil C= Chilled Water U= Upflow R= Upflow Air Pattern C= Chilled Water Air Pattern ... Main C= Chilled Water Air Pattern ... W= Water Cooled ... G= Glycol Cooled BA=208 ... U= Upflow Air Pattern ... W= Water Cooled
    Where can I get support for APC and MGE Products?
    Auto and Air Inverters ... Data Center Facility Cooling - Andover Continuum or TAC Vista ... EcoBreeze Air Economizers ... Environmental Monitoring Unit ... Fluid Coolers ... High-Density Cooling Enclosures ... InRoom Direct Expansion InRow Chilled Water InRow Direct Expansion ... Installation Services ... Mounting Hardware ... Portable Cooling ... Power Distribution Units ... Rack- mount Transfer Switches ... Room Cooling Accessories ... Row Cooling Accessories ... Software Installation ... Stationary Power Distribution Units ... Uniflair Chilled Water ... Wall - mount Transfer Switches
    How to navigate through an Network Air FM unit display
    ... through an Network Air FM unit display. ... ACFM, Network Air , ir40. ... identify the hardware installed in this System ... ... the coil configuration installed in the Modules ... Direct expansion (DX ... ... MultiCool® ( chilled water) and ... ... of the return air and the dew ... ... of the return air . ... , then the cooling setpoint is used ... ... (PCIOMs) installed in the user ... Installation ... of air filters installed in the Modules ... ... recommended for typical installations . Air ... avoid over- cooling while dehumidifying. When the unit is in dehumidification ...
    Network Air FM unit spare parts list
    Network Air FM unit spare parts list Install Please contact Cooling Tech Support to ... ... Cable Lower ( Upflow ) ... /Water & Air LL ... CAT5 for EXP unit Duct Collar Upflow Filter Air 30% UF ... DF 5/ Unit 756 X 325 ... Filter Air 85% UF ... DF 5/ Unit 756 X 325 ... ... FIRE DETECTOR - UPFLOW ... KW W/ AIR DEFLECTORS ... KW W/ AIR DEFLECTORS ... KW W/ AIR DEFLECTORS ... KW W/ AIR DEFLECTORS ... KW W/ AIR DEFLECTORS ... (for outdoor unit ) ... FM35-50 UNIT WIRING DOWNFLOW ... " Teflon FM units
    EPW9 APC ISX EPO Actuator Switch; product specifications and installation
    EPW9 APC ISX EPO Actuator Switch; product specifications and installation ... The wall mount assembly consists of a mechanical actuator which switches 9 sets of normally open contacts. Eight of the contacts are rated for 24V and intended to connect across the “Dry Contact-Normally Open” EPO signal terminals of an InfraStruXure power and cooling base building block. The ninth contact is rated for 240v and can be used to shunt trip an external device such as a breaker. ... See the Installation Manual for the EPW9 for complete installation instructions (990-1611A) attached below.
    What is the purpose behind an EcoAisle Ducted System.
    ... feature allows the compatibility with room or external cooling systems , by providing a direct return air path to the return of the cooling system ...
    Refrigerant charging table for a Uniflair Unit
    ... for a Uniflair Unit . Install . ... -cooled DX units must be connected ... ... condensers must have discharge and liquid lines ... Install all refrigerant lines ... ... refrigerant lines/ chilled water piping are free from debris. ... be short and direct as possible. ... refrigerant pipes are installed with proper supports ... ... brazing field- installed copper refrigeration lines ... Discharge Line Sizing Discharge lines must be ... Discharge lines must be ... ... pressure drops in discharge lines are up ... Horizontal discharge lines must be ... .Trap the discharge line at the ... Calculating Total Discharge Line Size: Discharge Line Size— ...
    What are the operational conditions for an InRoom (Stulz) Unit
    ... (Stulz) Unit Install ... precision air conditioning units operate within the ... Chilled water-/ cooling water pipes: ... piping between the cooling unit and the air ... ... condenser and the cooling unit : 5 m ... is below the cooling unit Return air conditions for evaporator ... Return air conditions for cooling ... Cooling fluid (DX): 30% Glycol ... Chilled water medium (CW): 0% Glycol ... Downflow units with an external static pressure: 20 Pa (0.08 in w g) Upflow units with an external static pressure: 50 Pa (0.20 in w g)
    Results 1 - 10 of 50