Browse FAQs



Is there a depth extender for the rear or front of NetShelter SX cabinets? Is there a way to bay the rear of cabinets that are different depths?
The roof of the depth extender is not load bearing. Do not run cables , troughs or ladders atop the depth extenders.
What width cable ladder will attach to the pass-through data cable partitions?
NOTE: AR8164ABLK and AR8165ABLK both contain hardware that allow cable ladder to attach to the NetShelter partitions and troughs .
Is there a NetShelter Accessory Compatibility Chart that shows which NetShelter accessories, UPS, PDU, Symmetra, NetBotz, Air or KVM fit into a specific cabinet?
... door, doors, vertical, horizontal, cable manager, management ... , manager, ladder , shelf, trough , partition, bracket,
Can the horizontal cable troughs ar8008blk and ar8016ablk be used in conjunction with vertical cable managers ar7580a, AR7585 and AR7588?
We need to know if the tabs on the horizontal cable troughs will mount to the rails when vertical cable managers ar7580a, AR7585 or ...
What is the capacity (in Lbs.) of NetShelter Cable Ladder, or the capacity of a structure containing cable ladder?
Issue: Information regarding the capacity of NetShelter Cable Ladder is required.
Do the NetShelter SX 12U and 18U cabinets have the standard SX roof, or are they different?
Issue: A customer may want to use ladder or troughs atop these cabinets and needs to know if the roofs are different.
Can I run cables over the SC? If so, how many?
Yes, there is a cable support bridge trough available as an accessory (acac10021).
Uniflair BACnet (Building Automation and Control Networks)
All the units must be fitted with a RS485 card, trough that they are connected to the RS485 serial cable .
InRow RC Standard and Optional Features
Power Trough (Overhead power distribution between racks) Data Partion Trough (Allows removal of RC unit without disrupting cabling )


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.