Technical FAQs

Ask a Question

Filter results

    Network Air FM fan curve chart
    Issue: Network Air FM fan curve chart.
    Why do I need refrigerant traps in my piping?
    All Air Cooled Cooling Units ... Oil is easily trapped in a discharge muffler, so it should be placed in the horizontal or downflow portion of the piping, as close to the compressor as possible. ... A: Whenever a condenser is located above the compressor, an inverted trap or check valve should be installed at the condenser inlet to prevent liquid refrigerant from flowing backwards into the compressor during off cycles.
    APC Schneider Cooling Unit Identification
    APC Cooling Unit identification. All Cooling Units . APC Unit Identification ... Humidifier D= Downflow ... Humidifier D= Downflow ... Humidifier D= Downflow D= Downflow DF= Downflow E= Fan Coil/Evap ... ... Condenser/Condensing Unit (Not Current ... ... CN= Condensing Unit ... Centrifugal C= Fan Cycle F= Fan Speed ... Condenser/Condensing Unit /Drycooler ( ... ... = Air Cooled Fan Speed Control ... Humidifier D= Downflow ... 60 D= Downflow ... 60 D= Downflow D= Downflow ... MA= 600/3/60 D= Downflow ... (Ceiling Mount Unit ) ... (Ceiling Mount Unit ) ... MA= 6575/3/60 D= Downflow ... D= Downflow ... D= Downflow
    What are the operational conditions for an InRoom (Stulz) Unit
    Downflow units with an external static pressure: 20 Pa (0.08 in w g)
    How to replace a NetworkAIR FM Series Filter Replacement
    Filters are replaceable through the front of the upflow unit , and through the top of the downflow unit .
    Network Air FM unit spare parts list
    0w2677c KIT FM35-50 UNIT WIRING DOWNFLOW
    Are the 600mm unit fans hot swappable?
    Issue: Are the 600mm unit fans hot swappable?
    What is the power factor (PF) of the ACSC cooling unit?
    Most of the PF comes from the compressors. The unit fan power bus rectifiers are PF corrected.
    On the replacement NetShelter CX fan tray the center pin of the DC connector has a larger o.d.
    When comparing the replacement fan unit (0M ... replacement has a fan switch, and ... connector on the fan appears to be different.
    Results 1 - 10 of 50