Technical FAQs

Ask a Question

Filter results

    Which SmartSlot accessories are supported by the Galaxy 3500 (g3500) UPS?
    It can utilize some of the 3 -phase Symmetra bit register/ ... properly if you are not in a 3:3 configuration.
    Which UPS models are compatible with AP9622 Modbus/Building Management Integration Card? Where are the UPS bit registers AP9622?
    : The Galaxy 3500 UPS is supported by the ... however some specific Symmetra 3 -phase registers ... unless in a 3:3 configuration.
    Why are the battery charge LEDs flashing on a Smart-UPS?
    Battery Charge LED Bar ... Smart- UPS , Smart- UPS Online ... All Smart- UPS models with model ... ... line, the runtime remaining (calculated ... the Smart- UPS microprocessor) must ... AT LEAST two minutes more than the low battery signal warning time ... If the UPS calculates the runtime remaining as being less than 2 minutes more than the low battery signal time, the battery charge graph LEDs ... ... Reset the low battery signal time to ...
    How to configure the SRC 5,6,8 & 10 KVA UPS Models External Battery Packs using the LCD display
    ... Configuration of SRC battery packs via the ... Smart- UPS Online Batteries need to be ... added to the UPS in order for ... to properly calculate runtime ... the number of battery strings through the ... 3 . Press the ... ... number of attached battery packs. ... setup the external battery packs, please ... (Ah of battery ) x (total number of batteries ). ... 16pcs of 5ah battery in series ( ... ... of 100 AH batteries in series(for 5 KVA ), the ... Example 3 : If there ... 16pcs of 5ah battery in series ( ... ... 16pcs of 5ah battery )
    Why is my actual UPS runtime different from the quoted runtime on the APC web page?
    ... is my actual UPS runtime different from the quoted runtime on the APC ... Smart- UPS ... is my actual UPS runtime different from the quoted runtime on the APC ... The runtime shown on the ... determine the actual runtime achieved in anyone ... ... temperature of the battery within its environment ... therefore the available runtime . ... Age of the battery ... - A new battery will only reach ... a two or three discharge and charge ... Temperature & battery life ... capacity of a battery will increase at ... % for every 10 deg Celsius rise ... Recharging the battery ... - Whilst a battery will recharge to ...
    What type of battery could I use with the Galaxy VS UPS?
    ... Galaxy VS, 3 Phase UPS , Uninterrupted Power Supply, 10 kVA ,15 kVA ,20 kVA , 20 kVA ,30 kVA ,40kva, ... What type of battery could I use ... the Galaxy VS UPS ?, battery , gvsups100kgs gvsups10kfs ...
    Smart-UPS SRC 5k, 6k, 8k and 10 KVA FAQ
    ... 4A/ 3 A/6A/ ... actual condition to keep the battery at full state, thus extending the battery life.
    PowerChute Network Shutdown reports "Available runtime has been exceeded".
    For conditions 3 and 4 below ... ... duration of 2 minutes (this consists of a 10 second OS shutdown ... Condition 3 for VMware: ... than the Low Battery Duration minus two minutes configured for the UPS . ... of a low battery condition, PowerChute ... sequence before the UPS powers off. ... time required is 3 minutes and Low Battery Duration is 4 minutes , the Available Runtime has been Exceeded ... ... configured for the UPS On Battery event plus the ... greater than the Runtime Remaining on the UPS minus two minutes .
    Why does Symmetra LX see only half of my installed battery modules?
    ... see all installed batteries when only one ... ... half of the batteries . ... intelligence module monitors battery bays 1, 3 , 5, ... , 8, 10 , &12 ... ... removed, the battery count may decrease depending on which battery slots are populated with battery modules. ... delay reporting changed battery module counts for 2 minutes , allowing the ... ... longer than 2 minutes , a decrease ... number of installed battery modules may be ... Please note that while some battery modules may not be ... the proper amount of runtime should the UPS have to operate using its battery supply.
    Matrix-UPS run time theory
    ... method the Matrix UPS calculates its estimated runtime ? Matrix UPS ... on the Matrix UPS calculates the " ... ... Age of the batteries ... . Type of battery (lead acid ... 3 . Number of battery packs ... . Type of battery packs (i ... ... applied to the UPS . ... a fully charged battery begins to discharge ... ... again when the battery capacity is almost ... ... To allow the UPS to predict when the battery will be exhausted ... ... curve, the UPS will be able ... Three of the four battery constants are set depending on the battery type (i ...
    Results 1 - 10 of 50