Technical FAQs

Ask a Question

Filter results

    How to navigate through an Network Air FM unit display
    ... NetworkAIR FM DX Precision Air Conditioner . Direct expansion (DX) ... ... MultiCool® ( chilled water ) and DX ... ... , then the cooling setpoint is used ... Water ... capacity uses one compressor and half of ... ... avoid over- cooling while dehumidifying. ... coil and both compressors . ... All refrigerant is directed through the expansion valve which feeds ... ... in which the compressors are engaged to ... hours that each compressor runs. ... in which the compressors are engaged. ... in which the compressors are engaged should ... ... used in the direct expansion refrigeration system. ...
    General functions of a MicroAC control platform DG3
    ... complete management of precision air-conditioners , both in direct expansion versions (with 1 or 2 compressors ), with ... valve on the cooling battery).
    APC Schneider Cooling Unit Identification
    APC Cooling Unit identification. All Cooling Units. ... FM Air/ Water /Glycol E= Expansion A= Air ... W= Water Cooled F= Water Cooled D= Water Cooled ... G= Glycol Cooled ... B= Glycol Cooled ... P= Glycol Cooled ... W= Hot Water ... Humidifier D= Downflow ... coil C= Chilled Water ... Humidifier D= Downflow C= Chilled Water ... Main C= Chilled Water W= Water Cooled ... G= Glycol Cooled BA=208 ... ... Humidifier D= Downflow W= Water Cooled ... G= Glycol Cooled D= Downflow
    Did APC purchase the AirFlow Company?
    Data Center Cooling ... be able to direct you to your ... American Power Conversion Expands Availability Solutions with Acquisition of Airflow Company Precision Cooling Acquisition Deepens Opportunities ... , a leading precision cooling equipment manufacturer, ... ... , highly efficient cooling solutions," ... ... entry into the precision cooling business while leveraging ... competitive position and drive synergistic growth. ... ... 800 million global precision cooling market. ... growth rate of greater than 30 percent ... ... are caused by cooling problems. Precision cooling solutions are specifically ... A precision cooling device goes beyond commercial building air conditioning or "comfort cooling " equipment to ... ... ceiling-mounted precision cooling systems as ...
    What are the operational conditions for an InRoom (Stulz) Unit
    The InRoom precision air conditioning units operate within ... Chilled water -/ cooling water pipes: Maximum water head pressure: ... ... piping between the cooling unit and the ... ... condenser and the cooling unit: 5 ... is below the cooling unit Entering water temperature (EWT ... Leaving water temperature (LWT) for CW coil: 12°C (53.6°F) ... Cooling fluid (DX): 30% Glycol ... Chilled water medium (CW): 0% Glycol ... Downflow units with an external static pressure: 20 Pa (0.08 in w g)
    Refrigerant charging table for a Uniflair Unit
    ... refrigerant lines/ chilled water piping are free ... ... be short and direct as possible. ... proper refrigeration/ AC vibration clamps. ... return to the compressor . ... ) of the compressor to ensure that ... ... back to the compressor during shutdown Liquid lines must be sized to ensure sufficient refrigerant flow to the expansion device and to minimize pressure drop. ... 5. Start the compressor , and complete the charging process. ... to avoid compressor damage.
    AirFlow CCT CW to DX Change Over
    Data Center Cooling ... In the event there is a need to run a Legacy Airflow product (CCT, or TC) in direct expansion (DX) mode while shutting down or doing maintenance on the chilled water (CW) system, below is the proper way to do a CW temp switch over. ... mode below the current water temp. This will cause the compressor (s) to come on as long as there is a demand for cooling . ... : Attached are documents regarding External Chilled Water Supply (ECWS) and its operation.
    acpa4000 Spare Parts List
    ... % 370vac ( compressor 0p4582 COMPRESSOR ROTARY 115/ ... (PANASONIC style compressor ... 6326A Condensate Pump EC -400 Little ... ... this with the water sensor pn# ... 0M-2470 Condenser Fan ( fan only 490-1045 Condenser Fan Box Sub Assy ( fan housing assy ... 870-3663 Evaporator Fan Box Assy ( fan only 490-1046 Evaporator Fan Box Sub Assy ( fan w/ housing assy ... 540-0088 Switch Thermal Overload Protector (for compressor pecker head ... 875-0853 Water Carry-Over-Kit (Air Dam kit 870-0656 0M-0844 Water Sensor Kit For acpa4000
    Where can I get support for APC and MGE Products?
    AC Power ... Data Center Facility Cooling - Andover Continuum or TAC Vista ... High-Density Cooling Enclosures ... InRoom Direct Expansion InRow Chilled Water InRow Direct Expansion ... Portable Cooling ... Room Cooling Accessories ... Row Cooling Accessories ... SmartSlot Expansion Chassis ... Uniflair Chilled Water
    Why do I need refrigerant traps in my piping?
    ... All Air Cooled Cooling Units Data Center Cooling ... both during the compressor on and off ... ... back to the compressor head, causing ... ... discharge of the compressor to the inlet ... ... lines will reduce compressor capacity and increase compressor work. ... returned to the compressor . ... muffler to my air conditioner ? ... the horizontal or downflow portion of the ... close to the compressor as possible. A: Whenever a condenser is located above the compressor , an inverted trap or check valve should be installed at the condenser inlet to prevent liquid refrigerant from flowing backwards into the compressor during off cycles.
    Results 1 - 10 of 50