Browse FAQs



APC Schneider Cooling Unit Identification
APC Cooling Unit identification. All Cooling Units. ... FM Air/ Water /Glycol E= Expansion A= Air ... W= Water Cooled F= Water Cooled D= Water Cooled ... G= Glycol Cooled ... B= Glycol Cooled ... P= Glycol Cooled ... W= Hot Water ... Humidifier D= Downflow ... coil C= Chilled Water ... Humidifier D= Downflow C= Chilled Water ... Main C= Chilled Water W= Water Cooled ... G= Glycol Cooled BA=208 ... ... Humidifier D= Downflow W= Water Cooled ... G= Glycol Cooled D= Downflow
General functions of a MicroAC control platform DG3
... control for the complete management of precision air-conditioners , both in direct expansion versions (with ... valve on the cooling battery).
How to navigate through an Network Air FM unit display
... NetworkAIR FM DX Precision Air Conditioner . Direct expansion (DX) ... ... MultiCool® ( chilled water ) and DX ... ... , then the cooling setpoint is used ... Water ... avoid over- cooling while dehumidifying. ... All refrigerant is directed through the expansion valve which feeds ... ... used in the direct expansion refrigeration system. ... ... the modes ( cooling , reheat, ... ... begins when an Expansion Module loses communication ... ... expires, the Expansion Module will shut ... ... or set the Expansion Modules to continue ... ... for fluid- cooled options ... of fluid- cooled option.
What are the operational conditions for an InRoom (Stulz) Unit
The InRoom precision air conditioning units operate within ... Chilled water -/ cooling water pipes: Maximum water head pressure: ... ... piping between the cooling unit and the ... ... condenser and the cooling unit: 5 ... is below the cooling unit Entering water temperature (EWT ... Leaving water temperature (LWT) for CW coil: 12°C (53.6°F) ... Cooling fluid (DX): 30% Glycol ... Chilled water medium (CW): 0% Glycol ... Downflow units with an external static pressure: 20 Pa (0.08 in w g)
Did APC purchase the AirFlow Company?
Data Center Cooling ... be able to direct you to your ... American Power Conversion Expands Availability Solutions with Acquisition of Airflow Company Precision Cooling Acquisition Deepens Opportunities ... , a leading precision cooling equipment manufacturer, ... ... , highly efficient cooling solutions," ... ... entry into the precision cooling business while leveraging ... ... 800 million global precision cooling market. ... growth rate of greater than 30 percent ... ... are caused by cooling problems. Precision cooling solutions are specifically ... A precision cooling device goes beyond commercial building air conditioning or "comfort cooling " equipment to ... ... ceiling-mounted precision cooling systems as ... ... its highly efficient cooling products, which ...
Uniflair Manual Start Up and Shut Down (PCO1)
If an alarm is indicated, consult the Uniflair Chilled Water and Direct Expansion Operation and Maintenance manual.
Where can I get support for APC and MGE Products?
AC Power ... Data Center Facility Cooling - Andover Continuum or TAC Vista ... High-Density Cooling Enclosures ... InRoom Direct Expansion InRow Chilled Water InRow Direct Expansion ... Portable Cooling ... Room Cooling Accessories ... Row Cooling Accessories ... SmartSlot Expansion Chassis ... Uniflair Chilled Water
Refrigerant charging table for a Uniflair Unit
• All refrigerant lines/ chilled water piping are free from debris. • All refrigerant lines should be short and direct as possible. ... Isolate piping from structural surfaces using proper refrigeration/ AC vibration clamps.
Video: How to reset an Air Filter Run Hours violation alarm on a Uniflair Unit
Uniflair, run, hours, violation, Chilled water , DX, Expansion , Direct
What is the difference between an InRow RP, InRow RD (600mm), and InRow RC (600mm)?
The minimum required kW for 1 direct expansion unit is 12kw and 12kw for chilled water . There should also be a consideration regarding humidity control.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.