Technical FAQs

Ask a Question

Filter results

    Rack PDU 2G (AP8XXX) Network Port Sharing Information
    General information regarding the Network Port Sharing (NPS ... Rack Power Distribution ... interested in Network Port Sharing (giving ... General information ... to the detailed information sections below. ... About the Network Port Sharing Feature ... use the Network Port Sharing feature to ... manage up to four Rack PDUs using ... ... "Out" ports on the Rack ... ... support the Network Port Sharing Feature. ... , 1 to 4 , used to ... ... Connect up to four Rack PDUs. ... IN/OUT ports on each end of the ... ... terminators per Network Port Sharing group. ... how many Network Port Sharing groups you ...
    APC Environmental Sensors FAQ
    ... Maximum length of cable - 330 ft ... of leak sensing cable - 400 ft ... Maximum length of cable - 330 ft ... Maximum length of cable - 330 ft ... Maximum length of cable - 330 ft ... Maximum length of cable - 330 ft ... Maximum length of cable - 330 ft ... -5 ethernet cables and either RJ45 ... or a patch panel . ... discrete connectors for each APC sensor, ... ... within the max cable length above. ... A-Link ports of the AP9319 ... ... ends of the cable , required for proper data transmission on the cable .
    ACSC1XX Spare Parts List
    CABLE ASSY RELATIVE HUMIDITY ... CABLE ASSY RELATIVE HUMIDITY ... CABLE ASSY Temperature Humidity ... CABLE ASSY Temperature Sensor CABLE ASSY TEMPERATURE SENSORS CABLE ASSY TEMPERATURE SENSORS ... ... Ceiling Tile Adapter 24 " - Spare ... ... WIDE INPUT, FULL SIGNALS, BLACK DUCTING KIT 24 INCH IR5 ... SWITCH BULK MOUNT 4 " MNL ... 1 3/ 4 "GD X ... (for power cable at the bottom ... ... for side door panels ) ... & black cat5e cable ) 4 ... /Probe EMU Cable ASSY - Spare ... ... BLACK AP9335TH ( holds sensor cables ) 4 WIRE TIE 4 X.1 ... 1 U Airflow Management Blanking ...
    What is Modbus and How does it work?
    ... can also write information to the Slaves ... ... main controller or data gathering system, ... ... supervisory control and data acquisition (SCADA ... ... a single serial cable connecting the serial ports on two devices ... The data is sent as ... Each bit is sent ... ... the actual raw data being Each block of 4 bits is represented ... Each block of 8 ... How is data stored in Standard ... Information is stored in ... Slave device in four different tables. ... coils and registers each have a read ... Each table has 9999 ... Each coil or contact ... and assigned a data address between
    Phase Sources on Symmetra LX PDU Panel SYAPD1
    ... my SYAPD1 PDU panel so that I ... ... less than the total frame rating. Each phase should supply ... loads must be distributed properly by the ... ... the standard PDU Panel provided on rack ... ... -30r ( 4 -pin twist ... ... the SYAPD1 PDU Panel sources from Phase ... ... the SYAPD1 PDU Panel sources from Phase ... ... the load on each phase; this information can be accessed ... The information in this document, in addition to the load percentages given by the UPS display, should be enough to balance the load properly across the output phases.
    ap9620 Legacy Communications Card (LCC) Compatibility
    ... DB9 simple signaling cable using pin 3 ... ... the UPS serial port is required. 3 U ... the ap9620's USB port functionality, only ... ... serial or USB cable . ... to the serial port of the PC ... 940-1524 cable . ... to the serial port of the PC ... ... to the serial port of the PC ... ... Setup > Serial port . ... ), 8 data bits, no ... ... valuable UPS firmware information can be found ... ... You still have full UPS control via ... Please refer to the attached document for the expected functionality of the LCC with each unit mentioned above. For the most up to date functionality information , please refer to the
    acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
    ... hardware and ceiling panel required to extend ... ... hardware and ceiling panel required to extend ... Ceiling panel assemblies come with ... ... begin the ceiling panel ... critical nature of data center loads, ... 4 . Wear appropriate ... Each of the following ... ... Containment System; each panel is connected by ... to completely remove each panel . ... flange nuts on each doorframe upright to ... ... install two 21 U side panels onto each NetShelter VS ( ... ... grounding studs on each 21U side panel ... Align each bracket’s mounting hole ... ... flange nut for each bracket. Ceiling Panels ... Types of ceiling panels and required hardware
    Video: How do I configure APC Network Management Card network settings?
    ... -APC serial cable to your device ... Configuration Cable Part Number ... -9 serial port 940-0024 ... ... connecting the correct cable , start the ... Configure port settings appropriately for ... Commonly used port settings are as ... COM Port Settings ... a DB9 serial port 2400 bps, 8 data bits, no ... ... bps, 8 data bits, no ... ... bps, 8 data bits, no ... manual for more information 2nd Generation Rack ... bps, 8 data bits, no ... ... bps, 8 data bits, no ... ... bps, 8 data bits, no ... Apply the port settings to establish ...
    Netbotz Version 1 Appliances - Ethernet Compliance and Feature Set
    ... the data sheet info on the ethernet ... ... LU3X31FT Single- Port 3 V 10 ... ... /TIA 568 cabling guidelines to ANSI ... 100 Mbits/s PLL, combined with the digital adaptive equalizer, robustly handles variations in rise-fall time, excessive attenuation due to channel loss, duty-cycle distortion, crosstalk, and baseline wander. ... IEEE 802.3 u Clause 28 compliant auto-negotiation for full 10m and 100m control. ... Full LED support. ... 10 Mbits/s PLL exceeding tolerances for both preamble and data jitter.
    Why is my equipment dropped or rebooted while connected to my Smart-UPS?
    4 ) Ground Loop ... - Each UPS is limited ... ... is capable of handling the amount of ... ... fed by different panels , there is ... Incorrect serial cable ... that the serial cable attached to the ... (COM) Port on the back ... is the correct cable . ... end of the cable that attaches into the UPS COM port . ... " followed by 4 digits and sometimes ... ... -APC serial cable will cause an ... ... use the serial cable provided by APC ... an optional APC cable for your specific ... ... All APC serial cables are proprietary and ... non-APC cable will work with ...
    Results 1 - 10 of 50