Technical FAQs

Ask a Question

Filter results

    Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
    ... such as a Rack PDU, AV ... ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... ... in to be powered down or cause ... ... PX 250/ 500 , you have ... ... AP9635, and Rack PDU 2G ... ... PX 250/ 500 , you have ... ... result in unexpected operation of your AP9635 ... within Control Panel. On a Rack PDU specifically, ... will resume normal operation , at which ... ... PX 250/ 500 , you have ...
    Where can I get support for APC and MGE Products?
    AC Power AV Power Filters Basic Rack PDU Cabinet Power Distribution Configurable Power Accessories Configurable Power Distribution Data Center Facility Cooling - ... Data Center Facility Power - PowerLogic ION ... Data Center Software Integration Kits Data Center University Data Distribution Cable Desktop Notebook Stands ... FRP/Ferroresonant Power Supply ... InfraStruxure for Large Data Centers ... InfraStruxure for Medium Data Centers ... InfraStruxure for Small Data Centers Laptop Power Adapters Metered Rack PDU ... by-Outlet Rack PDU Mobile Notebook Stands Modular Power Accessories Modular Power Distribution NetBotz 500 NetBotz Access Control NetBotz Rack Access ... NetShelter Open Frame Rack Accessories Open Frame Racks
    Did APC purchase the AirFlow Company?
    Data Center Cooling American Power Conversion Expands Availability Solutions with Acquisition of Airflow Company ... 2000 - American Power Conversion (NASDAQ ... ... today’s datacenters are power and heat. As the power density continues to ... Similar to power disruptions, temperature ... ... through the precise control of temperature and ... ... patented Symmetra® Power Array(TM ... -phase uninterruptible power supply (UPS ... S and DC power system company Advance Power , as well ... ... their global datacenter power and cooling needs ... ... ABL and Advance Power’s operations ; the timely ... rates in the power protection industry and ... ... of the Company’s licensing of certain patent ... from General Signal Power Systems and from ...
    Creating an Aggregate Device within the KVM Access Software
    ... case of utilizing Rack PDU Power Integration, creating ... user to manage power to that specific ... ... do the necessary power down, they ... ... have 300 node license but have 300 ... ... has a dual power supply so in ... a 900 node license to cover all ... ... Key in the information so that the ... name and password information under certain single ... ... Provide any additional information in the Contact ... ... ) Set the Power Control Options as outlined ... ... enable confirmation for power operation ... enable delay for power operation , and set the power on/ power off delay field ...
    INFORMATION BULLETIN: Potential Issue with AP8XXX series Rack Power Distribution Units with rpdu2g v6.0.9 firmware
    ... the selected port for: 57600 bps, 8 data bits, no parity, 1 stop bit, and no flow control .
    Alert Actions for NetBotz Version 2 Appliances
    Control Pod or third party intelligent power strip Play Audio ... the alert NetBotz 500 , Camera Pod ... attached external, power speakers Call Web ... Sends customer alert information via the Web ...
    NetBotz version 2 Power Control Pod Maximums
    NetBotz version 2 Power Control Pod Maximums ... Up to 16 power control pods can be connected to a NetBotz 500 Up to 4 power control pods can be connected to a NetBotz 420 (wall or rack ) The NetBotz 320 (wall or rack ) does not support a USB connection and hence does not support any power control pods.
    Can I monitor and control APC's rack mount PDUs serially with a Netbotz version 2 or version 3 appliance and rPDU 3.x firmware?
    ... I monitor and control APC's rack mount PDUs serially ... APC rack PDUs ... 2 420 and 500 units with a ... version-3 rack mount 450 and ... ap79xx series of rack mount PDUs. Connecting the nbac0226 USB to serial cable to the bot and connecting the 940-0144 cable from the nbac0226 to the RJ9 serial port of the PDU will allow control of the outlets of the ap79xx. ... Additional info : ... NetBotz 500 supports up to 16 rPDU's.
    Rack PDU 2G (AP8XXX) Network Port Sharing Information
    General information regarding the Network ... Capability of AP8XXX Rack PDU models Rack Power Distribution AP8XXX Rack PDU series only General information ... to the detailed information sections below. ... up to four Rack PDUs using only ... ... by connecting the Rack PDUs via the ... ports on the Rack PDU front panel ... All Rack PDUs in the ... using the same Rack PDU firmware revision ... ... uniquely identify the Rack PDUs in a ... ... two or more Rack PDUs are connected ... ... up to four Rack PDUs. ... or AP89XX series Rack PDU was manufactured ... ... or AP89XX series Rack PDU was manufactured ...
    Scripting with APC by Schneider Electric Switched Rack Power Distribution Units (PDUs)
    ... or automating outlet control on Switched Rack PDUs. AP79XX Switched Rack PDUs ... , AP89XX Switched Rack PDUs ... ) AP8XXX series Rack PDUs) ... to automate outlet control actions using scripting ... The following information is available for ... , and AP89XX Rack PDU devices. AP79XX Switched Rack PDU Series ... Schneider Electric Switched Rack PDUs, beginning ... to automate outlet control . ... receive the following information upon accessing the ... American Power Conversion Rack PDU ap7900 v ... ... Unit ID: Rack PDU ... with the Switched Rack PDU. ... Alternatively, AP79XX Rack PDUs offer outlet control via Simple Network ...
    Results 1 - 10 of 50