Technical FAQs

Ask a Question

Filter results

    Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
    ... such as a Rack PDU, AV ... ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... ... in to be powered down or cause ... ... AP9635, and Rack PDU 2G ... ... result in unexpected operation of your AP9635 ... within Control Panel. On a Rack PDU specifically, ... will resume normal operation , at which ... ... result in unexpected operation of your AP9635 ... The Local Control Console allows you ... ... parity, 8 data bits, 1 ... and no flow control . If
    Creating an Aggregate Device within the KVM Access Software
    ... case of utilizing Rack PDU Power Integration, creating ... user to manage power to that specific ... ... do the necessary power down, they ... ... have 300 node license but have 300 ... ... has a dual power supply so in ... a 900 node license to cover all ... ... Key in the information so that the ... name and password information under certain single ... ... Provide any additional information in the Contact ... ... ) Set the Power Control Options as outlined ... ... enable confirmation for power operation ... enable delay for power operation , and set the power on/ power off delay field ...
    INFORMATION BULLETIN: Potential Issue with AP8XXX series Rack Power Distribution Units with rpdu2g v6.0.9 firmware
    ... the selected port for: 57600 bps, 8 data bits, no parity, 1 stop bit, and no flow control .
    NetBotz 750 | Physical Description
    - Rack Monitor 750 ... line inlet Input power connection. ... Switched Outlet Provides power to a device ... ... Provide communications and power to connected devices ... sensor pods, rack access pods, ... 5 Rack Access Ports* ... 8 10/ 100 /1000 Network Port Provides a connection to the network. ... See for additional information . 9 Private LAN Provides a 10/ 100 /1000 connection to a private local area network and 48 VDC to an attached device. ... 13 Relay Output Used for connecting relay- controlled external devices. ... 16 Power LED Illuminates when the unit is receiving power .
    Rack PDU 2G (AP8XXX) Network Port Sharing Information
    General information regarding the Network ... Capability of AP8XXX Rack PDU models Rack Power Distribution AP8XXX Rack PDU series only General information ... to the detailed information sections below. ... up to four Rack PDUs using only ... ... by connecting the Rack PDUs via the ... ports on the Rack PDU front panel ... All Rack PDUs in the ... using the same Rack PDU firmware revision ... ... uniquely identify the Rack PDUs in a ... ... two or more Rack PDUs are connected ... ... up to four Rack PDUs. ... or AP89XX series Rack PDU was manufactured ... ... or AP89XX series Rack PDU was manufactured ...
    Scripting with APC by Schneider Electric Switched Rack Power Distribution Units (PDUs)
    ... or automating outlet control on Switched Rack PDUs. AP79XX Switched Rack PDUs ... , AP89XX Switched Rack PDUs ... ) AP8XXX series Rack PDUs) ... to automate outlet control actions using scripting ... The following information is available for ... , and AP89XX Rack PDU devices. AP79XX Switched Rack PDU Series ... Schneider Electric Switched Rack PDUs, beginning ... to automate outlet control . ... receive the following information upon accessing the ... American Power Conversion Rack PDU ap7900 v ... ... Unit ID: Rack PDU ... with the Switched Rack PDU. ... Alternatively, AP79XX Rack PDUs offer outlet control via Simple Network ...
    Rating and Use of UL489 Molded Case Circuit Breakers in APC Rack Power Distribution Products
    ... Breakers in APC Rack Power Distribution Products Rack Power Distribution Rack PDU models with ... ... are used in rack power distribution units. While there are some circuit breakers that are Listed and marked for 100 % use, circuit breaker size and the required enclosure space preclude use of these circuit breakers in Rack PDUs. Below is an excerpt from the UL Guide information for UL 489 Molded Case Circuit Breakers: ... Unless otherwise marked, circuit breakers should not be loaded to exceed 80% of their current rating, where in normal operation the load will continue for three hours or more.
    Can I change the input plug or reduce the cord length on my Rack Power Distribution Unit (Rack PDU) or Rack Automatic Transfer Switch (ATS)?
    Rack Power Distribution Unit ( ... Rack Automatic Transfer Switch ... ... warranty on a Rack PDU or Rack ATS if a licensed electrician is used ... For more information on UL markings ... APC Rack ATS and Rack PDU products have not been evaluated by safety agencies for hardwiring in the field and as such, customer modification of these products for hard wiring cannot be supported. Hardwiring these products would require removing the cover to gain access to the internal power connections. ... Additionally, removing the cover and modifying the input power wiring can create dangerous shock hazards that may result in death or serious injury.
    INFORMATION BULLETIN - Using Global Outlet Groups simultaneously between AP79XX and AP8XXX series Rack PDUs with the same multicast IP range causes AP79XX PDU not to boot properly
    American Power Conversion Network Management ... ... All Rights Reserved Rack PDU APP v ... Rack Power Distribution AP79XX Switched Rack PDU AP89XX Switched Rack PDU 2G ... AP79XX series Switched Rack PDUs. ... generations of Switched Rack PDU are enabled ... ... groups of Switched Rack PDUs are utilizing ... ... groups of Switched Rack PDUs are on ... ... generations of Switched Rack PDU active in ... ... different generation of Rack PDU to your ... ... the AP79XX series Rack PDU which will ... ... each series of Rack PDU, and ... ... is where the information is located. ... .0. 100 OutletGroupMulticastIPAddr=224.0.0. 100 ... MULTICAST_IP_A=224.0.0. 100
    What does the "Reset ATS Controller" command accomplish on a Next Gen Rack Automatic Transfer Switch (ATS)?
    What does the "Reset ATS Controller" command accomplish on a Next Gen Rack Automatic Transfer Switch (ATS)? ... Rack Power Distribution - Automatic Transfer Switch ... This information is provided to users wishing to understand what the "Reset ATS Controller" command does and the functions it performs. ... The ATS is resetting and the CPU/microcontroller is not in control and able to maintain the output. ... Lastly, scenarios one and two also cover how the ATS powers up when a coldstart is performed.
    Results 1 - 10 of 50