Technical FAQs

Ask a Question

Filter results

    INFORMATION BULLETIN: Potential Issue with AP8XXX series Rack Power Distribution Units with rpdu2g v6.0.9 firmware
    Run a terminal program such as HyperTerminal, and configure ... data bits, no parity, 1 stop bit, and no flow control .
    Why is my AP561X KVM Switch Not Recognizing My Rack PDU for Power Management Integration?
    ... recognizing the attached Rack PDU for Power Management. ... IP KVM Switches support Rack PDU power integration for the ability to control outlets via the ... ... the user to power on/off ... or warrants a control action. Switched Rack PDU models including ... One or more of ... to utilize the Rack PDU Power Integration ... an APC Switched Rack PDU beginning with ... a supported Switched Rack PDU is the required AP5641 power management cable Your PDU has rpdu application 2.7.0 or higher
    Creating an Aggregate Device within the KVM Access Software
    ... KVM Access Management Software and why it ... KVM Access Software (ships with ... ... their KVM Access Software All software versions ... ports into a single Aggregate Device, ... counts as a single node, and only requires a single license. ... case of utilizing Rack PDU Power Integration, creating ... user to manage power to that specific ... ... through the Access Software . When a ... do the necessary power down, they ... ... has a dual power supply so in ... ... the KVM Access Software . 1 .) Within ... ... you are adding one of the specifically ... ... information under certain single sign on situations ...
    Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
    ... such as a Rack PDU, AV ... ... with the wrong application and you need ... load the correct application . ... Environmental Monitoring Unit 1 (AP9312TH) ... ... Network Management Card 1 - AP9617, ... ... Network Management Card 1 include (but ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... ... in to be powered down or cause ... ... pertain to your application . Symmetra 1 phase (Symmetra ... ... section on the software downloads page. ... link to the software downloads page is ...
    Rack PDU 2G (AP8XXX) Network Port Sharing Information
    ... Capability of AP8XXX Rack PDU models Rack Power Distribution AP8XXX Rack PDU series only ... ability to share one IP address via one network connection) ... up to four Rack PDUs using only one ... by connecting the Rack PDUs via the ... ports on the Rack PDU front panel ... All Rack PDUs in the ... using the same Rack PDU firmware revision ... in order to support the Network Port ... ... a number, 1 to 4, ... uniquely identify the Rack PDUs in a ... ... two or more Rack PDUs are connected to one another in a ... ... up to four Rack PDUs.
    How do Software Support & Extended Warranty contracts work for NetBotz?
    wnbwn004 - Extension of 1 year Software Support and Hardware Warranty for Rack Monitor nbrk0450 & nbrk0570 (Requires the purchase of the wnbwn002 initially)
    Network Management Card SNMP Support Overview
    ... Management Card SNMP Support Overview ... Network Management Card 1 - AP9617, ... ... Network Management Card 1 include (but ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP86XX ... ... Card's and their support for Simple Network ... ... Network Management Card 1 and 2 families ... (such as Rack PDUs, Rack Power Filter, Netbotz ... , etc) support snmpv1 and v ... ... for full device support . The ... formats and protocol operations that are incompatible ... ... strings and access control settings.
    Did APC purchase the AirFlow Company?
    Data Center Cooling ... purchased Airflow in 2000 and formed a ... American Power Conversion Expands Availability Solutions with Acquisition of Airflow Company ... October 23, 2000 - American Power Conversion (NASDAQ ... ... , global, one -stop shop ... ... today’s datacenters are power and heat. As the power density continues to ... Similar to power disruptions, temperature ... ... specifically designed for applications that are sensitive ... IT and telecommunications applications . ... through the precise control of temperature and ... ... a variety of applications including datacenters, ... ... solutions also offer one of the smallest ...
    Scripting with APC by Schneider Electric Switched Rack Power Distribution Units (PDUs)
    Switched Rack PDU 1 G, scripting, outlet control , CLI, ... line interface, rack PDU, rack PDU scripting, snmp, ...
    APC Security Advisory - Static Factory Password Vulnerability
    ... result in unauthorized control of these devices ... ... system and the application file for the ... ... or device has one of these cards ... ... to a newer application revision that has ... at the same application revision for those ... ... devices with network support are affected. ... Description AOS Rev APP Rev AOS Rev APP Rev Smart- ... ... mx28 110 Switched Rack PDU aos 116 ... ... The AOS and APP firmware revisions listed ... ... _hw02_ APP _REV. ... ... both AOS and APP revsions are available ... ... Description AOS Rev APP Rev AOS Rev APP Rev Smart- ... ... The AOS and APP firmware revisions listed ...
    Results 1 - 10 of 50