Technical FAQs

Ask a Question

Filter results

    How do software support contracts work for StruxureWare Data Center Expert.
    If you have an AP9465 StruxureWare Data Central Basic with an additional 100 node license and you want them to be under support for a ...
    Rating and Use of UL489 Molded Case Circuit Breakers in APC Rack Power Distribution Products
    ... Breakers in APC Rack Power Distribution Products Rack Power Distribution Rack PDU models with ... ... are used in rack power distribution units ... While there are some circuit breakers that are Listed and marked for 100 % use, circuit breaker size and the required enclosure space preclude use of these circuit breakers in Rack PDUs. Below is an excerpt from the UL Guide information for UL 489 Molded Case Circuit Breakers: ... Unless otherwise marked, circuit breakers should not be loaded to exceed 80% of their current rating, where in normal operation the load will continue for three hours or more.
    Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
    ... such as a Rack PDU, AV ... ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... ... AP9635, and Rack PDU 2G ... ... result in unexpected operation of your AP9635 ... On a Rack PDU specifically, ... will resume normal operation , at which ... ... result in unexpected operation of your AP9635 ... ... parity, 8 data bits, 1 ... ... result in unexpected operation of your AP9635 ... ... bps, 8 data bits, no ... ... result in unexpected operation of your AP9635 ...
    Can I change the input plug or reduce the cord length on my Rack Power Distribution Unit (Rack PDU) or Rack Automatic Transfer Switch (ATS)?
    Rack Power Distribution Unit ... Rack Automatic Transfer Switch (ATS) Models ... APC will continue to honor the product warranty on a Rack PDU or Rack ATS if a licensed electrician is used to change the input plug or provided the replacement plug has the equivalent ratings of the original APC supplied plug. ... For more information on UL markings, please see the attached document. ... APC Rack ATS and Rack PDU products have not been evaluated by safety agencies for hardwiring in the field and as such, customer modification of these products for hard wiring cannot be supported.
    Uniflair Humidifier Water Quality
    Data Center Cooling. Theory of operation ... to maintain the optimum concentration of dissolved ... ) Total hardness TH mg/l 100 (2 ) 100 Temporary hardness mg/l 60(3 ) 300 Iron + manganese mg/l Fe + Mn 0 0.2 Chlorides ppm Cl 0 30 Silica mg/l 0 20 Residual chloride mg/l 0 0.2 Calcium sulphate mg/l 0 100 Metallic impurities mg/l 0 0 Solvents, diluents, soaps, lubricants mg/l 0 0
    What is ETL?
    StruxureWare Data Center Operation ETL stands for Extract, ... ... tool that allows data to be transferred from one data source to another ... ... of ETL in Data Warehouses ... to load your data warehouse regularly so ... ... do this, data from one or ... copied into the data warehouse. ... The challenge in data warehouse environments is ... large volumes of data over many systems ... a new unified information base for business ... ... process of extracting data from source systems ... it into the data warehouse is commonly ... ETL, which stands for extraction, ... ... necessarily unique to data warehouse environments: ... Data has to be ...
    NetBotz 750 | Network Port Light Indicators
    - Rack Monitor 750 ... Link (10/ 100 /1000) LED ... The cable that connects the appliance to the network is disconnected or not functioning properly. ... Solid Green The appliance is connected to a network operating at 100 Megabits (Mb) per second or 1000 Mb/1 Gigabit (Gb) per second. ... Flashing Green The appliance is receiving or transmitting data packets at 1 Gb per second. Flashing Orange The appliance is receiving or transmitting data packets at 10 Mb or 100 Mb per second.
    Why is my ACRP excessively cycling?
    Data Center Cooling ... If there is empty rack space without blanking panels, the cold air flowing to the hot aisle will reduce the heat load that the RP is given. ... The cool setpoint controls the fan speed based on the maximum rack inlet temperature. The higher the rack inlet temperature is, the higher the fan speed will be (relative to the cool setpoint). ... In low load situations, the optimal setpoints often differ based on the specific room configuration.
    DAC, Cancoil Installation Manual
    ... Warranty and General Information ……… ... ... and Sequence of Operations ……… ... ... Cooled Condensers For information pertaining to product ... electrical and capacity data , please visit ... General Information ... efficient year round operation for low, ... ... record the following information in the space ... ... done by a licensed mechanical contractor in ... The following information may be used ... The data in the tables ... ... 2 degrees per 100 equivalent feet of ... 1 degree per 100 equivalent feet. ... and Sequence of Operations ... diagram for specific information regarding the model ... All hook-up, evacuation, testing and charging work must be done by a licensed refrigeration contractor.
    Results 1 - 10 of 50