Technical FAQs

Ask a Question

Filter results

    Why is my ACRP excessively cycling?
    Data Center Cooling ... Unless the system continues to operate for 5 - 10 minutes oil will be left in the system. ... If there is empty rack space without blanking panels, the cold air flowing to the hot aisle will reduce the heat load that the RP is given. ... The cool setpoint controls the fan speed based on the maximum rack inlet temperature. The higher the rack inlet temperature is, the higher the fan speed will be (relative to the cool setpoint). ... In low load situations, the optimal setpoints often differ based on the specific room configuration.
    Rack PDU 2G (AP8XXX) Network Port Sharing Information
    ... of communication issues, the maximum total length of cabling connecting Rack PDUs in a group should not exceed 10 meters.
    Why does StruxureWare Data Center Expert not accept my One Time passcode?
    StruxureWare Data Center Expert is not ... StruxureWare Data Center Expert ... StruxureWare Central / Data Center Expert all versions ... SturuxureWare Data Center Expert requires a 64 character license key that is ... passcode and the Data Center Expert's MAC address ... ... when purchasing a license key is not the actual license . ... passcode to a license key. ... AP9465 = StruxureWare Data Center Expert Basic ... ap9470 = StruxureWare Data Center Expert Standard ... AP9475 = StruxureWare Data Center Expert Enterprise ... AP94VMACT = StruxureWare Data Center Expert Virtual Machine ... SFDCOBASE = StruxureWare Data Center Operation ... a VM or Data Center Operation . 10 .
    Data Center Expert | Alarm "Device status may be inaccurate due to attempt to transfer DDF failed"
    StruxureWare Data Center Expert message " ... StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... Data Center Expert uses device ... to understand what information to poll from ... ... APC NMC, Data Center Expert will attempt ... ... occurs that causes Data Center Expert to reach ... 2) Data Center Expert attempts to ... ... Log into the Data Center Expert Desktop Client ... For additional information on passive connections ... ... be enabled for Data Center Expert to retrieve ... ... credentials listed within Data Center Expert. ... Log into the Data Center Expert desktop client ... ... -20, 10 .10. ...
    Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
    ... such as a Rack PDU, AV ... ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... ... AP9635, and Rack PDU 2G ... ... result in unexpected operation of your AP9635 ... On a Rack PDU specifically, ... will resume normal operation , at which ... ... result in unexpected operation of your AP9635 ... ... parity, 8 data bits, 1 ... 10 . Select option ... ... result in unexpected operation of your AP9635 ... ... bps, 8 data bits, no ...
    What Proximity Cards are supported by the NetBotz NBACS125 & NBACS1356 Rack Access Control Systems?
    The NBACS125 Rack Access Control appliance supports the following Proximity Cards ... Additional packs of 10 cards (ap9370- 10 ) can by purchased from APC by Schneider Electric. The NBACS1356 Rack Access Control appliance supports the following Proximity Cards ... For more information , see the product brochure below. ... : Pod Sharing with the NBACS125 / NBACS1356 Rack Access Control systems is NOT supported at this time
    APC Switched Rack PDUs - any pending outlet commands are lost when PDU Network Management Interface is rebooted
    Rack Power Distribution AP79XX Switched Rack PDU AP89XX Switched Rack PDU 2G AP86XX Switched Rack with Metering By ... ... connection to a Rack PDU powered by ... ... for more than 10 minutes ... Users rebooting their Rack PDU with outlet ... ... stored by the Rack PDU in Random ... Additional information on the network ... ... not power the Rack PDU's network connection by the same Rack PDU's outlets ( ... for longer than 10 minutes) - If the Rack PDU's network connection ... ... activated when the Rack PDU discovers it ... ... to reboot the Rack PDU to apply ... ... - if your Rack PDU's network connection ...
    Can I change the input plug or reduce the cord length on my Rack Power Distribution Unit (Rack PDU) or Rack Automatic Transfer Switch (ATS)?
    Rack Power Distribution Unit ... Rack Automatic Transfer Switch (ATS) Models ... APC will continue to honor the product warranty on a Rack PDU or Rack ATS if a licensed electrician is used to change the input plug or provided the replacement plug has the equivalent ratings of the original APC supplied plug. ... For more information on UL markings, please see the attached document. ... APC Rack ATS and Rack PDU products have not been evaluated by safety agencies for hardwiring in the field and as such, customer modification of these products for hard wiring cannot be supported.
    AP84XX, AP88XX, AP89XX, and AP86XX 2G Rack PDU LCD Backlight Behavior
    Rack Power Distribution ... span of the rack LCD display and ... ... remain on for 10 minutes. Then, 10 minutes after the last button is pushed, the backlight will turn off. The ... AP84XX series Metering by Outlet Rack PDUs require v6.1.0 rpdug app and higher and are being released in September, 2014. They cannot be downgraded. ... If it has been previously configured, you can find the IP address listed on the front display of the PDU under Main Menu->Software Info ->IP address.
    Video: How can I download Event, Data, Configuration, and Debug files from my Network Management Card?
    ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... ... download Event and Data logs from a ... ... require backup of data and/or ... ... .txt, data .txt, ... .txt, data .txt, ... screen to indicate data transfer). ... <space> data .txt 10 .) Type ... ... Export Logs ( data .txt, ... .txt and data .txt ... .txt, data .txt, ... ... and choose either Data ->Log ...
    Results 1 - 10 of 50