How to navigate through an Network Air FM unit display
Operation . ... MultiCool® ( chilled water) and ... Indicates the humidity control method. ... can control the humidity based on the relative humidity (RH • Relative humidity (RH ... and the return humidity value. ... near the environmental sensors , and is ... temperature and relative humidity of the room ... ... , then the cooling setpoint is used ... humidity is 40% ... ... when the remote sensor readings are used ... ... avoid over- cooling while dehumidifying. ... the modes ( cooling , reheat, ... ... System cannot begin operation until this delay ... ... It allows the sensors to obtain an ... Sensor setup